Site Level Dashboard
In this dashboard, the user can view the overview of the Site. Based on the configuration, respective KPI details are displayed in the
Overview
tab in the form of cards.Select the required
Site
from the hierarchy list and the following tabs are displayed in the dashboard:- Overview
- Areas
- Assets
NOTE:
To change the date or time period, refer to Change Date or Time Period.
Overview
The user can view the status of the Site and configured KPIs across the application under the selected Site and the top five underperforming assets on the selected time frame. The user can also view the active alerts with severity, actions taken, and the current status of the alert.
Site Overview

In the KPI trend chart, three lines indicate the three different KPI data, the solid lines indicate the historic data, and the dotted line indicates the extrapolated future projected data. Hover over the solid line and dotted line to view the KPI values with the corresponding date.
In the KPI trend chart, the user can view the Trend at the top and a sparkline view below. The user can change the date selection by using the selectors of 1/3/6 months, year to date [YTD], 1 year, and all. The user can use the sliding selector at the bottom to change the date selection.
NOTE:
- Click the [
] icon in the chart and click
Download SVG vector imageto download the chart in SVG vector image format. - Click the [
] icon in the chart and click
View in full screento view the chart in full screen.
The user can view the individual KPI graph of the
Top 5 Underperforming Assets
and the graph is displayed for the past 3 months. Hover the mouse over the chart to view the selected KPI value with the corresponding date. The user can also select the required KPI from the KPI drop-down list and the corresponding graph is displayed in the Past 3 Months
column.Top 5 Underperforming Assets

NOTE:
To customize the top 5 underperforming asset table, refer to Customize Top 5 Underperforming Assets Table.
Click the [
] icon on the required

Asset Name
to view the Asset Hierarchy
details.Asset Hierarchy details

The user can view all the active alerts with alert descriptions, severity, start date, action taken, and current status details. Click on the
Alert ID
to view the respective alert page.Active Alerts

Customize Table
Hover the mouse over the required column and click the [
] icon to customize the table with the following configurations:

- Column OptionsNOTE: The column options are applicable forAsset Namecolumn only.
- Pin Column: Hover the mouse over Pin Column and select the options from the drop-down list to pin the selected column. The column is pinned on the Data Table.
- Autosize This Column: Select theAutosize This Columnoption to resize the selected column width in the table.
- Autosize All Columns: Select theAutosize All Columnsoption to resize the column width of all columns in the table.
- Resize Columns: Select theResize Columnsoption to resize the column width of all columns to default size in the table.Pin Column
- Filter Data: Select the required checkboxes or provide the data on the Search box to filter the data.Filter Data
- Grid Option: Select or clear the required columns or provide the data in the Search box in the Data Table. Based on the selection, the customized Data Table is displayed.Grid OptionNOTE: The grid option is applicable forAsset Namecolumn only.
- Sorting: Click on the column header to sort the data in ascending or descending order.Sorting Data
The user can also pin the required column and filter the column heading from the table's global settings (
Columns
):- Filter Column: Select or deselect the required columns or provide the data in the Search box in the Data Table. Based on the selection, the customized Data Table is displayed.
Areas
The user can view the status of the Area on the Site. For example, Beneficiation has associated KPIs of Health Index, Reliability, Throughput, and Alert count. The associated KPIs are configured in the Dashboard Setup and are the same KPIs across the application.
NOTE:
To know about the card functionality, refer to Card Functionality.
Area Cards

Assets
The user can view summaries of the asset classes associated with this point in the hierarchy. Each card represents an Asset Class with rolled-up statuses. By selecting an individual
Asset Class
, the user can filter the list of assets available in the Asset Details
section. Click on the Asset Name
to view the corresponding Asset page.Asset Cards and Details

Provide Feedback