FT Activation Websocket Service Log

FT Activation Websocket Service Log

  1. Log file Location:
    <<Installation_Directory>>Program Files (x86)>Rockwell Automation>FactoryTalk Activation Websocket Service>service.log
    Log file
NOTE:
By default, the Websocket Service log is not generated unless the error occurs.
  1. To generate the log files in normal situation, user needs to change the log lever as required in
    WebsocketService.dll.config
    file.
    For example:
    To view the Debug log, change the log level value to '
    Debug
    ', as shown in the following figure:
    FT Activation WebSocket Config file
    FT Activation WebSocket Service Log
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal