Basic Pie Chart

Basic Pie Chart

  1. Open a Storyboard, hover the mouse on a chart tile and click the [] icon to maximize the tile.
  2. Click the [] icon. The Chart Settings window displays.
    View
    Under the Type tab, the list of available chart types display.
  3. Click [Pie Chart]. The available chart models display.
  4. Select the [Basic Pie] Chart from the Pie Chart section.
    Chart Settings
  5. Under the Configuration tab, provide the following properties:
    • Y-Axis: Select the desired attribute using the [] icon. User can add more than one Y-Axis values for this chart.
    • X-Axis: Select an attribute of date type using the [] icon.
    • Tooltip: User can select the values to be displayed on the tooltip.
      The Basic Pie Chart displays.
  6. Click [Apply].
    Chart Settings
    The Basic Pie Chart displays.
    Basic Pie Chart
  7. Click the [] icon to minimize the chart. The updated Storyboard displays
    Storyboard Updated
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal