Configure Login Settings

Configure Login Settings

  1. In the Login menu, the Admin can change the settings options for User login using toggle switches.
The following features can be made available during login:
  • Forgot Password
    - If enabled, a link appears on the login page in case the User has forgotten their credentials.
  • Remember Me
    - If enabled, a checkbox on the login page will allow the User to remain logged in between browser restarts until the session expires.
  • Verify Email
    - If enabled, this feature requires the User to verify their email address the first time they login. An email will be sent to the User's email asking for confirmation.
  • Login with Email
    - If enabled, user can login with Email.
  • Require SSL
    - SSL ensures that all communication between the web server and browser remains encrypted. Use the drop-down list to select one of the following options:
  • None: HTTPS is not required for any client IP address.
  • External Requests: localhost and private IP addresses can access the application without HTTPS.
  • All Requests: HTTPS is required for all IP addresses.
    Configure Login Settings
  1. Once all the changes are made to the settings using the toggle switches, click [Save] and a success message displays in the top center of the web browser.
  2. Click [Cancel] to discard any changes made.
  3. Once the Forgot Password link is enabled, the login page displays the [Forgot Password] link.
  4. Click [Forgot Password] to reset password.
    Forgot Password Option
  5. Enter Username or email and click [Submit].
    Password Reset
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal