Analyze Data

Analyze Data

Data Explorer provides analysis tools allowing you to plot process data in the following formats:
To use these analysis tools, do one of the following:
  • From the
    Analysis
    icon’s drop-down menu, select one of the following analysis types. You will be asked to define your data selection.
  • In the
    Value
    Statistics
    tab or other appropriate graphical tabs, select your data, right-click within the selection, and go to Analyze > one of the following analysis types.
If you want to analyze all the data, either do a Ctrl+a or click the
Select All
icon.
For the data represented in each analysis tool, the right-click > Plot/Analyze options are available.
NOTE:
Most plots can be pinned or displayed with particular filters (not all data). Most analysis plots do not include error/cut data. Users may select raw data from the Analysis icon at the Top of SolutionBuilder.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal