Export Calculator

Export Calculator

  • <filename>.calculator.xml - is an xml format script describing the streaming processing routines. This is a proprietary format loaded and processed by the Pavilion8 streaming calculation programs that executes as a microservice connected to an execution platform.
  • <filename>.calculator.log - includes a detailed description of the calculator export processing steps.
Note that by themselves without changing the filename or path that these files will be updated and in general overwritten. Alternatively, and it is recommended that filenames be modified to map to different, identifiable configurations and needs. Data is intended to be updated as needed in an interactive data science workflow so overwriting occurs without warning. The user will experience errors if overwriting a file that is open by other programs (for example, EXCEL) that lock a selected file.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal