Overriding Nominals on Analysis Plots
On either the prediction of output variables vs input variables or sensitivity of output variables vs input variables (model-based analysis features) users may adjust or override model nominal values. That is image a color model with five inputs. One plot may show how color responds when input1 is moved from its minimum to maximum, but this happens while input2 through input 5 are held at their nominal value. By overriding nominals, the user may shift every nominal and observe that five-dimensional color model from different states.
Users may adjust nominal values (temporarily) to gain increased model insight as desired. Values may be shifted graphically with individual input variable sliders or numerically with the values identified in the box. Note that nominal values beyond the modeled maximum or minimum are not accepted. Nominals may be reset with the adjacent [ ] reset button.
Provide Feedback