Model Definition Tab

Model Definition Tab

As on other features, Models may be saved or unsaved and renamed. Preference options are available on select model parameters for preferred default values. If filters are selected, then only filtered data is included in training and analysis functions and can also be leveraged on calculation export to specify how run-time data excluded via defined filters are handled automatically.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal