Launch Data Explorer

Launch Data Explorer

Once Data Explorer is installed:
  1. Launch the application using one of the following methods:
    • Double-click the Data Explorer shortcut icon on your desktop.
    • From your Windows Start menu, go to Rockwell Software > Data Explorer.
    • Double-click DataExplorer.exe located by default at C:\Program Files\Rockwell Software\FactoryTalk Analytics Data Explorer\FactoryTalk Analytics Data Explorer <version>.
      Create or Load Project
  2. In the Create or Load Project screen, do one of the following to define your project. A project is a place to save one or more datasets and, optionally, save view definitions with them.
    • Enter a new project name. The New Project radio button is selected by default.
    • Select the Load Existing Project radio button and either click [Browse…] to select an existing mpm project file or select one of the recently opened projects listed in the table.
  3. Click [OK]. The Data Explorer UI displays.
    Data Explorer UI
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal