Configure Custom Properties

Configure Custom Properties

To configure properties that were customized in Data Explorer before the import, click [Configure Properties]. You can perform the following tasks in this dialog. When finished, click [OK].
  • To toggle between displaying and not displaying a property label on plot pop-ups, click the property and click [Toggle Displayed]. Any property that is toggled to display (enabled star) means that the property value will be included wherever the name of the variable is rendered. For example, if there is a displayed property called
    units
    and for the variable flow, the units are
    gal/min
    , then the variable will be displayed as
    flow (gal/min)
    .
  • To add a custom property, click [Add] and define the property.
  • To remove a property, select the property and click [Remove].
    Configure Properties
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal