Windowing on Tabs

Windowing on Tabs

The Data Explorer display framework does allow for flexible arrangement of windows, where each window is a selected primary tab. By selecting the tab label (shown below as “TurbineEmissionsAnalyze” or “Trend Plot” or “High Power” (a filter) or “Statistics”) the user can drag each tab and reorder them by placing a dragged tab anywhere between existing tabs or the product boundary frame. Also if the product is not maximized, the user may drag a tab outside the product frame and create it as an exterior separate tab image available in a second screen or otherwise on the users primary screen. The Menu Bar options to split or close all are supported and extensions of these tab image capabilities.
Tabs
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal