Highlighting Data

Highlighting Data

You can highlight data in a plot or analysis tool using the Highlighter icon. Highlighting can be started graphically by using Alt-select and dragging a box around the data to be highlighted. This can occur multiple times. Use Shift-Alt-select-drag to unhighlight (graphically, also multiple unselect sections allowed). The master highlight icon allows users to undo-last, clear-all, and edit a highlight sequence set or convert to a retained filter.
  1. Click the
    Highlighter
    icon to open an
    Active Highlighter
    tab Click the Highlighter icon to open an Active Highlighter tab.
    Active Highlighter Tab
  2. From the
    Add Rule
    drop-down menu, select a type of highlight rule to add. You can choose from the following:
    • Data within a range of rows and times
    • Data within a specific set of statuses and values
    • Data within an allowed range or ranges of values
    • Data linked to an existing filter
  3. To save your rules for future use, click the
    Highlighter
    icon or select
    Save as a New Filter
    from the drop-down menu of the
    Highlighter
    icon. Access your saved rules by clicking the
    Open Projects Window
    icon and selecting the rules set. It will be listed as a Dataset Filter, which may be renamed from the Filter tab.
To add a new rule to the highlighter, click the
Highlighter
icon to open the
Active Highlighter
tab, and select your rule. Clicking
Edit
from the
Highlighter
icon’s drop-down menu also opens your list of rules.
To remove a highlight rule, select the rule in the
Active Highlighter
tab and click [Remove Selected].
Click [Toggle Include/Exclude] to toggle between applying and removing the selected highlighter rule on your data. You can also use the
Remove Last
and
Reapply Last
options from the drop-down menu for the same purpose.
To undo all highlights, click
Reset…
in the
Highlighter
icon’s drop-down menu.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal