Manage
Transformed Data
Transformed data (called
transforms) is any data that has been changed in some way (for example,
cut) since being imported, but the transformed data list also includes
raw data that has not been modified by transforms. All transforms
on the dataset are kept in one ordered list. This list includes
functions that you apply directly to the data and transforms that
are automatically generated by cuts. Transforms can be modified
or deleted. Any action that generates a transform can be undone
by deleting the transform. Therefore, no data is eliminated unless
deleted from the manifest explicitly.
Provide Feedback