Time
Merge Variables
In a dataset, the
variable types are date/time, numeric (real, integer, or double
precision), or string, and variable origins are raw, independent,
or computed.
Numerics and strings can be attached to a date/time
variable, or they can be unattached, without any date/time information.
You can change the date/time pointer of raw or independent columns
but not of computed columns A computed column inherits the date/time
pointer of the column from which it is transformed.
You can time merge all or some of the variables
in a dataset. You can select the date/times and the variables that
are unattached. When you merge a date/time variable, all other variables
that reference it are also merged; the original date/time variable
is removed from the after-transforms dataset and replaced with a
new merged time, and the date/ time pointers are changed to the
new merged time. When an unattached column is time merged, its values
are not changed, but its date/time pointer is set to the new merged
time variable.
Provide Feedback