General Information and Conventions

General Information and Conventions

Unless noted otherwise:
  • Transforms operate only on numeric values.
  • x refers to any numeric constant or variable, and var is any numeric variable.
  • dtVal is any date/time constant or variable, and dtVar is any date/time variable.
  • string is any string constant or variable, and stringVar is any string variable. String constants are surrounded by double quotes (") or single quotes (').
  • Output of transforms is a single real variable that can be the same as or different from an input variable.
Date/time constants are specified as date followed by time, separated by at least one space, surrounded by backslash (\) characters. The date and time must be in a form that the parser can recognize. The recommended form is \ mm/dd/yy hh:mm:ss.ttt \ with seconds and thousandths optional.
Date/time increments are specified as a value and a unit, surrounded by backslash (\) characters. The value is a real number. The unit can be milliseconds, seconds, minutes, hours, or days (but not months or years); it can be spelled out or abbreviated to the first unique character.
Some status transforms operate on a variable's status only, and some on its status and value.
Function and constant names are not case-sensitive. Sometimes we display and document them in uppercase or mixed case, but this is solely for ease of recognition.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal