- FactoryTalk Design Studio Help
- Programs, tasks, and routines
- Add-On Instructions
- FactoryTalk Design Studio Code editor
- Instructions
- Instruction set
Add an existing device
Add an existing device to a Backplane or Ethernet bus to assign its position in the bus.
To add an existing device:
- On the explorer bar, selectDevices.
- InDevicesexplorer, right-click a backplane from the list and then selectAdd device. TheAdd devicedialog box opens.
- InAdd device, selectFrom Project.
- Select a device from the list and then selectAdd.TIP: Only devices compatible with the bus are shown.
- In theOverviewview, selectOK. The device appears under the bus in Devices explorer.
Provide Feedback