- FactoryTalk Design Studio Help
- Programs, tasks, and routines
- Add-On Instructions
- FactoryTalk Design Studio Code editor
- Instructions
- Instruction set
Task syntax
This section describes the syntax for
FactoryTalk Design Studio
tasks.A task component defines a task in the controller project. You can configure up to 32 tasks in a ControlLogix or CompactLogix Controller project.
Provide Feedback