- FactoryTalk Design Studio Help
- Programs, tasks, and routines
- Add-On Instructions
- FactoryTalk Design Studio Code editor
- Instructions
- Instruction set
Close a project
Close a project when changes are complete or close a project in order to open another project.
- On the menu bar, selectFile > Close project.TIP: If autosave is in progress, "Saving" appears in the title bar next to the project name.
Provide Feedback