Delete a user-defined data type

Delete a user-defined data type

Delete user-defined data types from the Library Explorer.
Prerequisite
  • Remove or delete all instances of the user-defined data type
To delete a user-defined data type
  1. In
    Library
    , expand the
    Data Type
    folder.
  2. Right-click the data type and select
    Delete User Data Type.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.