Set Network Path in IntelliCENTER Dashboard

Set Network Path in IntelliCENTER Dashboard

Use the
Set Network Path
tab to set, modify, or clear the network path.
To set Network Path in IntelliCENTER Dashboard
  1. On the explorer bar, select Devices Icon
    Devices
    .
  2. Select the
    IntelliCENTER
    tab.
  3. In the
    IntelliCENTER
    explorer, select the
    IntelliCENTER Dashboard
    at the bottom of the explorer.
  4. In the
    IntelliCENTER Dashboard
    , select a lineup and then right-click and select
    Set Network Path
    .
  5. In the
    Set Network Path
    tab, select a network and either paste the network path or
    Browse
    to the desired path.
  6. Select
    Start Status Monitoring
    to start status monitoring the lineup. All network paths must be set to start status monitoring. If you do not want to start status monitoring, select
    Save and Close
    to save the network paths and continue working.
  • To clear a network path, use the Delete function.
  • For network paths that were previously setup, the
    Set Network Path
    tab changes to the
    Edit Network Path
    tab.
  • To communicate with the controller, Add a VPN driver.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.