- FactoryTalk Design Studio Help
- Programs, tasks, and routines
- Add-On Instructions
- FactoryTalk Design Studio Code editor
- Instructions
- Instruction set
Replace units
Use the
Replace unit
option to exchange an empty door with a Units-only dataset.Prerequisites
- Purchase and download the dataset folder.
- Unzip the dataset folder to your local drive.
- AFactoryTalk Design Studioproject with lineups.
- In theElevationview, right-click on an empty door and selectReplace unit.
- In theReplace Unitdialog box, selectBrowseunderDatabase.
- SelectImport.The empty Door is replaced with the imported unit-only dataset.
Provide Feedback