Launch the Unit Profile from the IntelliCENTER explorer

Launch the Unit Profile from the IntelliCENTER explorer

Use the
Unit Profile
tab to view detailed unit information in the IntelliCENTER lineup. View the:
  • device name
  • device type
  • IP address
  • MCC Network number
  • vendor code
  • product type
  • product code
  • major revision
  • minor revision
To launch the Unit Profile from the IntelliCENTER explorer
  1. On the explorer bar, select Devices Icon
    Devices
    .
  2. Select the
    IntelliCENTER
    tab.
  3. In the
    IntelliCENTER
    explorer, right-click a unit within a lineup and select
    Unit Profile
    to launch the Unit Profile and to view the unit information.
  4. (optional) To view unit documentation, under
    Documentation
    , select the
    Drawings
    ,
    Manuals
    , or
    Spares
    link.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.