- FactoryTalk Design Studio Help
- Programs, tasks, and routines
- Add-On Instructions
- FactoryTalk Design Studio Code editor
- Instructions
- Instruction set
Add multiple devices
FactoryTalk Design Studio provides the ability to add multiple devices in a single operation.
TIP:
Any changes made to devices while online will only impact the offline project.
To add multiple devices
:
- On the explorer bar, selectDevices.
- InDevicesexplorer, selectHamburger Menu, then selectNew device. TheAdd device to projectdialog box opens.TIP: To add a device to a specific Backplane or Ethernet Bus, right-click the Backplane or Ethernet Bus, then selectAdd device.TIP: To add a device from theDevice list, at the top of theDevice list, selectAdd device.
- InCategory filter, select each device category you want to add to the project.
- Select each catalog number that you want to add to the project. The devices you select will show in theDevices to addlist on the right of the dialog box.
- InCategory filter, select each device category you want to add to the project.
- (optional) In theDevices to addlist, increase the number to add that quantity of each device to the project.
- SelectContinue. TheAdd devices to projectwindow opens. The selected devices are listed in thePending to configurearea.
- Configure each of the devices in thePending to configurelist. When all the required fields for each device are configured properly, theFinishbutton becomes enabled.
- SelectFinishto add the devices to the project. Controllers are added as assigned. Devices other than controllers are added as unassigned.
Provide Feedback