Delete a device

Delete a device

Delete a device to remove the device from a bus and the project. Devices connected to buses below the deleted device are disconnected and returned to the
Unassigned
folder in
Device Explorer
.
TIP: Any changes made to devices while online will only impact the offline project.
To delete a device
  1. On the explorer bar, select Devices Icon
    Devices
    .
  2. In
    Devices
    , right-click a device in the list, then select Delete
    Delete
    . The device is removed from the project.
NOTE: When you delete a device, the devices assigned to it become unassigned, and on rack optimized devices, the device connection type reverts to the default setting, Data.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.