- FactoryTalk Design Studio Help
- Programs, tasks, and routines
- Add-On Instructions
- FactoryTalk Design Studio Code editor
- Instructions
- Instruction set
Device List
How do I open Device list?
- On the explorer bar, selectDevices.
- InDevicesexplorer, selectDevice list.
Use
Device list
to view, edit, and delete devices and to view tags for the devices in the project.The
Device list
displays information for each device:Column | Description |
---|---|
Name | The user-defined name of the device. |
Description | The user-defined description of the device. |
Revision | The firmware revision of the device. This value is read-only. |
Catalog Number | The catalog number of the device. Hover over the catalog number to view the catalog description. |
Category | The type of the device. |
Vendor | The manufacturer of the device. |
Electronic Keying | The electronic keying used for the module. Electronic keying compares the module defined in the project to the installed module. If keying fails, a fault occurs. Valid values are Exact Match, Compatible Module, and Disable Keying. For detailed information on Electronic Keying, see Electronic Keying in Logix5000 Control Systems Application Technique, publication LOGIX-AT001.Electronic Keying options include:
|
TIP:
- To open the profile of a device, inDevice list, right-click the device and selectOpen device properties.Overviewview opens.
Provide Feedback