- FactoryTalk Design Studio Help
- Programs, tasks, and routines
- Add-On Instructions
- FactoryTalk Design Studio Code editor
- Instructions
- Instruction set
Import Stratix device configuration
Import a
Stratix
device configuration to restore a device to a previous configuration. The configuration contains either one or two configuration files.- On the explorer bar, selectDevices.
- InDevices, right-click aStratixdevice, and then selectProperties.
- InProperties, selectSave/Restore, then selectImport.
- InImport, complete the following steps:
- In theConfig fileview, selectBrowseto navigate to and import theconfig.textorstartup-config.cfgfile.
- SelectOpen, then selectNext.
- (optional) If the device also requires a Vlan file, in theVlan fileview, selectBrowseto navigate to and import thevlan.datfile.
- (optional) SelectOpen, then selectImport.
- SelectOK.
Provide Feedback