Configure a program

Configure a program

A program is configured as a main or fault routine and you have the option to inhibit or enable the program. To configure a program, create a program from the System or Execution explorer.
To configure a program
  1. In the
    Properties
    pane, select the
    Configuration
    tab.
  2. In
    Configuration
    , the program is configured as either a main or fault routine:
    • Main Routine
      . The program is configured as a main routine that executes the logic when the program triggers.
      Main Routine
      contains the value . If the program is configured as a fault routine,
      Main Routine
      contains the value .
    • Fault routine
      . The program is configured as a fault routine that executes fault handling logic when the program fault occurs.
      Fault Routine
      contains the value . If the program is configured as a main routine,
      Fault Routine
      contains the value .
  3. Inhibit Program
    . Position the switch to Toggle On Position
    On
    to prevent the controller from performing this program. Position the switch to Toggle Off Position
    Off
    to enable the controller to perform the program.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.