- FactoryTalk Design Studio Help
- Programs, tasks, and routines
- Add-On Instructions
- FactoryTalk Design Studio Code editor
- Instructions
- Instruction set
Object icons
This table defines the icons in the FactoryTalk Design System.
Indicator | Meaning | |
---|---|---|
Online and offline | ![]() | Online indicator for nodes such as programs, routines, and devices. |
![]() | Offline indicator for nodes such as programs, routines, and devices. | |
![]() | Indicates a mix of nodes, some online and some offline. A dashed circle appears around an element's icon indicates that this node contains child nodes that have an offline-only or online-only state that is different from the parent node. Expand the child nodes to see the differences in these states for the child elements. Note that this icon is only shown while online. | |
Folders | ![]() | Folder. |
![]() | Folder with child elements in a mixed online state. | |
Routines | ![]() | Ladder routine. |
![]() | Ladder routine that is inherited. An inherited element inherits behaviors from its definition and any inherited definition. When a definition is updated, all instances and inherited definitions are also updated. | |
![]() | Ladder routine that is inherited, and an override has been applied. See Override Smart Object elements for more information on overrides. | |
Programs | ![]() | Program. |
![]() | Program that is inherited. | |
![]() | Program that is overridden. | |
![]() | Program with child elements in a mixed online state. | |
![]() | Program that is inherited and that has child elements in a mixed online state. | |
![]() | Program that is overridden and that has child elements in a mixed online state. | |
Smart Objects | ![]() | Standalone (non-inherited) Smart Object. |
![]() | Smart Object definition. | |
![]() | Smart Object that is inherited. | |
![]() | Smart Object that has child elements in a mixed online state. | |
![]() | Smart Object that is inherited and has child elements in a mixed online state. | |
Tags and parameters | ![]() | Tag. |
![]() | An inherited tag. | |
![]() | An overridden tag. | |
Tasks | ![]() | Periodic task. |
![]() | Continuous task. | |
![]() | Event task. | |
![]() | Task that has child elements in a mixed online state. | |
Add-On Instructions | ![]() | Add-On Instruction. |
![]() | EnableInFalse ladder routine Add-On Instruction. | |
![]() | Prescan Add-On Instruction. | |
Data type | ![]() | Data type. |
Devices | ![]() | I-O module. |
![]() | Ethernet bridge adapter module. | |
![]() | Communication module. | |
![]() | Controller. | |
![]() | Non-Ethernet module. | |
![]() | Backplane. | |
![]() | Ethernet module. | |
![]() | Ethernet bridge adapter module that has child elements in a mixed online state. | |
![]() | Controller that has child elements in a mixed online state. | |
![]() | Backplane that has child elements in a mixed online state. | |
![]() | Ethernet module that has child elements in a mixed online state. |
Provide Feedback