File Average (AVE)

File Average (AVE)

The AVE instruction calculates the mean of a set of values.
IMPORTANT: Make sure the Length does not cause the instruction to exceed the specified Dimension to vary. If this happens, the destination will be incorrect. For more information, see Viewing an Array as a Block of Memory.
If an overflow occurs during expression evaluation, the instructions reads past the end of an array, the instruction sets the ER bit and stops execution
Available Languages
Ladder Diagram
Ladder_FileAverage(AVE)_v1
Operands
There are data conversion rules for mixed data types within an instruction. See Data Conversion.
Ladder Diagram
Operand
Type
Format
Description
Array Tag
SINT
INT
DINT
REAL
tag
Find the average of the values in this array
specify the first element of the group of elements to average
Do not use CONTROL.POS in the subscript
Dimension to vary
DINT
immediate
(0, 1, 2)
Which dimension to use
the order of the dimensions is: array[0,1,2]
Destination
SINT
INT
DINT
REAL
tag
Result of the operation
Control
CONTROL
tag
Control structure for the operation
Length
DINT
immediate
Number of elements of the array to average
Position
DINT
immediate
Offset into the specified array which identifies the current element that the instruction is accessing.
initial value is typically 0
Affects Math Status Flags
Major/Minor Faults
None specific to this instruction. See Common Attributes for operand related faults.
Execution
Ladder Diagram
Condition/State
Action Taken
Prescan
The .EN bit is cleared.
The .DN bit is cleared.
If .ER bit is zero during prescan, all the control bits (.DN, .EN, .EU, .EM, .UL, .IN and .FD) will be cleared to zero.
Rung-condition-in is false.
See AVE Flow Chart (False)
Rung-condition-in is true.
The AVE instruction calculates the average by adding all the specified elements in the array and dividing by the number of elements.
Postscan
N/A.
AVE Flow Chart (False)
RSL5K_AVE Flow Chart False
Example 1
RSL5K_AVE Example 1
Ladder Diagram
FTStudio AVE EX1 V1
Example 2
RSL5K_AVE Example 2
Ladder Diagram
FTStudio AVE EX2 V1
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.