- FactoryTalk Design Studio Help
- Programs, tasks, and routines
- Add-On Instructions
- FactoryTalk Design Studio Code editor
- Instructions
- Instruction set
Valid Operators
The following are the valid operators.
Operator | Description | Allowed in | |||||
---|---|---|---|---|---|---|---|
Array Index | FSC | CMP | FAL | CPT | Safety | ||
+ | add | X | X | X | X | X | X |
- | subtract/negate | X | X | X | X | X | X |
* | multiply | X | X | X | X | X | X |
/ | divide | X | X | X | X | X | X |
= | equal | X | X | X | |||
< | less than | X | X | X | |||
<= | less than or equal | X | X | X | |||
> | greater than | X | X | X | |||
>= | greater than or equal | X | X | X | |||
<> | not equal | X | X | X | |||
** | exponent (x to y) | X | X | X | X | ||
&& | Logical AND | X | X | X | |||
|| | Logical OR | X | X | X | |||
^^ | Logical XOR | X | X | X | |||
! | Logical NOT | X | X | X | |||
ABS | absolute value | X | X | X | X | X | |
ACS | arc cosine | X | X | X | X | ||
AND | bitwise AND | X | X | X | X | X | X |
ASN | arc sine | X | X | X | X | ||
ATN | arc tangent | X | X | X | X | ||
COS | cosine | X | X | X | X | ||
DEG | radians to degrees | X | X | X | X | ||
FRD | BCD to integer | X | X | X | X | X | |
IsINF | Is infinity | X | X | ||||
IsNAN | Is not a number | X | X | ||||
LN | natural log | X | X | X | X | ||
LOG | log base 10 | X | X | X | X | ||
MOD | modulo-divide | X | X | X | X | X | |
NOT | bitwise NOT | X | X | X | X | X | X |
OR | bitwise OR | X | X | X | X | X | X |
RAD | degrees to radians | X | X | X | X | ||
SIN | sine | X | X | X | X | ||
SQR | square root | X | X | X | X | X | |
TAN | tangent | X | X | X | X | ||
TOD | integer to BCD | X | X | X | X | X | |
TRN | truncate | X | X | X | X | ||
XOR | bitwise exclusive OR | X | X | X | X | X | X |
Provide Feedback