- FactoryTalk Design Studio Help
- Programs, tasks, and routines
- Add-On Instructions
- FactoryTalk Design Studio Code editor
- Instructions
- Instruction set
Negate (NEG)
When enabled, the NEG instruction and operator subtract the Source value from zero.
Available Languages
Ladder Diagram
_v1.png/_jcr_content/renditions/original)
Operands
IMPORTANT:
Unexpected operation may occur if:
- Output tag operands are overwritten
- Members of a structure operand are overwritten
- Except when specified, structure operands are shared by multiple instructions.
There are data conversion rules for mixing numeric data types within an instruction. See Data conversions.
Ladder Diagram
Operand | Data Type | Format | Description |
---|---|---|---|
Source | SINT INT DINT LINT USINT UINT UDINT ULINT REAL LREAL | immediate tag | Value to negate |
Dest | SINT INT DINT LINT USINT UINT UDINT ULINT REAL LREAL | tag | Tag to store result of the instruction. |
Affects Math Status Flags
See Math status flags.
Major/Minor Faults
None specific to this instruction. See Index through arrays for array-indexing faults.
Execution
Ladder Diagram
Condition/State | Action Taken |
---|---|
Prescan | N/A |
Rung-condition-in is false | Set Rung-condition-out to Rung-condition-in. |
Rung-condition-in is true | Set Rung-condition-out to Rung-condition-in. Dest = 0 - Source. |
Postscan | N/A |
Examples
Ladder Diagram

Provide Feedback