Always False (AFI)

Always False (AFI)

The AFI instruction sets the EnableOut to false.
Available Languages
Ladder Diagram
Ladder Diagram_Always False (AFI)_v1
Operands
Ladder Diagram
None
Affects Math Status Flags
No
Major/Minor Faults
None specific to this instruction. See Common Attributes for operand-related faults
Execution
All conditions below the thick solid line can only occur during Normal Scan mode.
Condition
Action
Prescan
N/A
Rung-condition-in is false
Clear EnableOut to false.
Rung-condition-in is true
Clear EnableOut to false.
Postscan
N/A
Examples
Ladder Diagram
Use the AFI instruction to temporarily disable a rung while you are debugging a program. AFI disables all the instructions on this rung.
FTStudio-AFI-LD-EX-V1
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.