- FactoryTalk Design Studio Help
- Programs, tasks, and routines
- Add-On Instructions
- FactoryTalk Design Studio Code editor
- Instructions
- Instruction set
Sequencer Instructions
Sequencer instructions monitor consistent and repeatable operations.
Available Instructions
Ladder Diagram
If you want to | Use this instruction |
---|---|
Detect when a step is complete. | |
Set output conditions for the next step. | |
Load reference conditions into sequencer arrays |
The
bold
data types indicate optimal data types. An instruction executes faster and requires less memory if all the operands of the instruction use the same optimal data type, typically DINT or REAL.Provide Feedback