- FactoryTalk Design Studio Help
- Programs, tasks, and routines
- Add-On Instructions
- FactoryTalk Design Studio Code editor
- Instructions
- Instruction set
Set the device path
Use the
Set device path
dialog to set, modify, or clear the device path that specifies the target controller for the deploy operation.- On the explorer bar, selectDevices.
- InDevicesexplorer, right-click the controller and selectSet controller path.
- On theSet device pathdialog, select a target controller.
- SelectOKto save the communications path as the current device path.
Provide Feedback