FactoryTalk Linx and FactoryTalk Logix Echo binding to port 44818
The EtherNet/IP Encapsulation protocol defines a reserved UDP port (number AF12 hexadecimal; number 44818 decimal) which every EtherNet/IP device must support for the device to display in browse. By default,
FactoryTalk Linx
doesn't listen on this port until the Listen on EtherNet/IP encapsulated ports
checkbox is selected.FactoryTalk Edge Gateway
running on a workstation can also listen on this port, resulting in a race condition: the application that starts first aquires the port, and that application's identity is the one exposed to a browse. Since the FactoryTalk Edge Gateway
application also acquires the matching EtherNet/IP TCP port (number AF12 hexadecimal; number 44818 decimal), all EtherNet/IP communications will be directed to FactoryTalk Edge Gateway
.This port is occupied by
FactoryTalk Logix Echo
also. So, when the user uses the FactoryTalk Logix Echo
to simulate RA controllers and selects Smart Detection
then the Auto device and model
does not work and no devices are discovered. Workaround for this is to open the Windows Task Manager
, then in the Processes
tab , select the FactoryTalk Logix Echo
and Click End Task
.Perform the following steps to prevent FactoryTalk Linx from binding to port 44818:
- Launch theFactoryTalk Administration Console. Select the Local FactoryTalk directory.
- Within theCommunicationstab, right-click onEtherNet, Ethernetand selectProperties.
- Within theAdvancedtab, ensure that theListen on EtherNet/IP encapsulation portscheckbox is unchecked.
- ClickApply, then clickOk.
- Restart theFactoryTalk Linxservice.
Provide Feedback