Develop a color-coded alarm dashboard

Develop a color-coded alarm dashboard

Create a multilingual interface that displays color-coded alarms and enables you to acknowledge and confirm them.
Application example
NOTE:
Download a sample project:
ColorCodedAlarmGrid.zip
Prerequisites
In
FactoryTalk Optix Studio
, select
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal