Deploy a FactoryTalk Optix Application from a USB drive

To deploy a
FactoryTalk Optix Application
from a USB drive, move the file to the client device and run the file.
  1. To deploy a
    FactoryTalk Optix Application
    from a USB drive
  2. Move the file from the USB drive to the client device.
  3. Run
    FactoryTalk Optix Application
    on the client system:
    • On
      Windows®
      client devices, double-click
      FTOptixRuntime.exe
      .
    • On Linux client devices, in the terminal, navigate to the
      FTOptixRuntime
      file folder and enter
      ./FTOptixRuntime
      .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.