OPC UA

OPC UA

FactoryTalk Optix Studio
is compliant with the OPC UA (OPC Unified Architecture) standard and can communicate with any OPC UA client or server.
TIP: Devices with a configured
FactoryTalk Optix Application
can operate as an OPC UA client or server.
Use these components to develop your application logic:
  • OPC UA server object
  • OPC UA client objects
  • OPC UA nodes
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal