- Getting started
- Creating projects
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Configure the editor grid
Configure the grid in the editor to show or hide the grid, align objects in the grid, and size the grid.
- InProject view, double-click a container object, or select .The editor opens in a new tab.
- In the editor toolbar, selectGrid settings
- Select the option to configure the grid:
- Grid Visible. Toggle showing the grid in the editor.
- Snap to grid. Align the edges of objects with the grid.
- Grid size. Specify the size of the grid in pixels.
grid
editor grid
Provide Feedback