Create the UIPopulator NetLogic

Create the UIPopulator NetLogic

Create a NetLogic that automatically creates UI elements based on the Model objects properties.
Prerequisites
Set the default external code editor. See Set the default code editor.
  1. To create the UIPopulator NetLogic
  2. In
    Project view
    , right-click
    VerticalLayout1
    and select
    New
    Runtime NetLogic
    .
  3. Hover-over the NetLogic, select
    Edit
    , and enter
    UIPopulator
    .
  4. Double-click the NetLogic.
    The external code editor opens.
  5. In the code editor, replace the existing code with the following code:
    using System.Linq; using FTOptix.HMIProject; using FTOptix.UI; using UAManagedCore; using OpcUa = UAManagedCore.OpcUa; public class UIPopulator : FTOptix.NetLogic.BaseNetLogic { public override void Start() { // Get the Model variable of the ListBox modelObjectVariable = LogicObject.Get<IUAVariable>("ModelObject"); // Subscribe to the VariableChange event modelObjectVariable.VariableChange += ModelObjectVariable_VariableChange; // Build the UI based on the selected item BuildUI(modelObjectVariable.Value); } private void ModelObjectVariable_VariableChange(object sender, VariableChangeEventArgs e) { // Every time the ModelObject variable changes, rebuild the UI BuildUI(e.NewValue); } public override void Stop() { // Destroy the variable change event modelObjectVariable.VariableChange -= ModelObjectVariable_VariableChange; } private void BuildUI(NodeId modelObjectNodeId) { // Get the VerticalContainer that will hold the UI elements var verticalContainer = (ColumnLayout)Owner; // Get the ModelObject of the VerticalLayout from the NodeId var modelObject = InformationModel.Get(modelObjectNodeId); // Clear all the children of the VerticalContainer foreach (var child in verticalContainer.Children.OfType<Item>()) { child.Delete(); } // Create the UI elements based on the DataType of the children of the ModelObject foreach (var objectProperty in modelObject.Children.OfType<IUAVariable>()) { Item uiObject; if (objectProperty.DataType == OpcUa.DataTypes.Boolean) uiObject = MakeSwitch(objectProperty); else if (objectProperty.DataType == OpcUa.DataTypes.String) uiObject = MakeTextBox(objectProperty); else if (objectProperty.DataType == OpcUa.DataTypes.Int32) uiObject = MakeLinearGauge(objectProperty); else if (objectProperty.DataType == OpcUa.DataTypes.Float) uiObject = MakeCircularGauge(objectProperty); else if (objectProperty.DataType == FTOptix.Core.DataTypes.ResourceUri) uiObject = MakeImage(objectProperty); else uiObject = MakeTextBox(objectProperty); // Add the UI element to the VerticalContainer if (uiObject != null) verticalContainer.Add(uiObject); } } private static Panel MakeBaseContainer(IUAVariable variable) { // Create a Panel to hold the UI element var container = InformationModel.MakeObject<Panel>("ControlContainer"); container.Height = 50; container.HorizontalAlignment = HorizontalAlignment.Stretch; // Create a Label to show the name of the variable var label = InformationModel.MakeObject<Label>("Label"); label.VerticalAlignment = VerticalAlignment.Center; label.LeftMargin = 20; label.Text = variable.BrowseName; // Add the Label to the Panel container.Add(label); return container; } private static Item MakeSwitch(IUAVariable variable) { // Create a base container var container = MakeBaseContainer(variable); var mySwitch = InformationModel.MakeObject<Switch>("Switch"); mySwitch.HorizontalAlignment = HorizontalAlignment.Right; mySwitch.VerticalAlignment = VerticalAlignment.Center; mySwitch.RightMargin = 40; // Bind the Checked property of the Switch to the variable MakeDataBind(mySwitch.Children.Get<IUAVariable>("Checked"), variable); // Add the Switch to the container container.Add(mySwitch); return container; } private static Item MakeTextBox(IUAVariable variable) { // Create a base container var container = MakeBaseContainer(variable); var textBox = InformationModel.MakeObject<TextBox>("TextBox"); textBox.HorizontalAlignment = HorizontalAlignment.Right; textBox.VerticalAlignment = VerticalAlignment.Center; textBox.RightMargin = 40; // Bind the Text property of the TextBox to the variable MakeDataBind(textBox.Children.Get<IUAVariable>("Text"), variable); // Add the TextBox to the container container.Add(textBox); return container; } private static Item MakeCircularGauge(IUAVariable variable) { // Create a base container var container = MakeBaseContainer(variable); container.Height = 180; // Create a CircularGauge var circularGauge = InformationModel.MakeObject<CircularGauge>("CircularGauge"); circularGauge.Width = 140; circularGauge.HorizontalAlignment = HorizontalAlignment.Right; circularGauge.VerticalAlignment = VerticalAlignment.Stretch; circularGauge.RightMargin = 40; circularGauge.TopMargin = 20; // Bind the Value property of the CircularGauge to the variable MakeDataBind(circularGauge.Children.Get<IUAVariable>("Value"), variable); // Add the CircularGauge to the container container.Add(circularGauge); return container; } private static Item MakeLinearGauge(IUAVariable variable) { // Create a base container var container = MakeBaseContainer(variable); container.Height = 150; // Create a LinearGauge var linearGauge = InformationModel.MakeObject<LinearGauge>("LinearGauge"); linearGauge.Width = 140; linearGauge.Height = 35; linearGauge.HorizontalAlignment = HorizontalAlignment.Right; linearGauge.VerticalAlignment = VerticalAlignment.Center; linearGauge.RightMargin = 40; linearGauge.TopMargin = 20; // Bind the Value property of the LinearGauge to the variable MakeDataBind(linearGauge.Children.Get<IUAVariable>("Value"), variable); // Add the LinearGauge to the container container.Add(linearGauge); return container; } private static Item MakeImage(IUAVariable variable) { // Create the image object var image = InformationModel.MakeObject<Image>("Image"); image.HorizontalAlignment = HorizontalAlignment.Center; image.Width = 100; image.Height = 100; image.TopMargin = 20; image.BottomMargin = 20; // Set the path property of the image object image.Path = new FTOptix.Core.ResourceUri(variable.Value); return image; } private static void MakeDataBind(IUAVariable property, IUAVariable targetVariable) { // Set the DynamicLink to a variable as ReadWrite property.SetDynamicLink(targetVariable, FTOptix.CoreBase.DynamicLinkMode.ReadWrite); } private IUAVariable modelObjectVariable; }
  6. Save the code.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.