Station Runtime Lite (S)
This S example shows you a system architecture using a panel PC and two controllers.
This example architecture has the following components:
- Single HMI station (panel PC) with typical HMI functionality
- Communicates with aRockwell Automation®controller and a third-party controller
- Logs data to an internal database
- Requires event logging, alarming, recipes, and basic PDF reporting
The following picture shows example runtime sizing for a package that includes these application components.
Provide Feedback