disable-keying

Disable Keying

Disable Keying indicates that the keying attributes are not considered when attempting to communicate with a device. With Disable Keying, communication can occur with a device other than the type specified in the project.
ATTENTION:
Be extremely cautious when using Disable Keying; if used incorrect, this option can lead to personal injury or death, property damage, or economic loss.
We
strongly recommend
that you
do not use
Disable Keying.
If you use Disable Keying, you must take full responsibility for understanding whether the device being used can fulfill the functional requirements of the application.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal