Identify attributes from codes
This table provides an alphabetical list of all Motion Axis Attributes specific to the CIP Drive data type. The table identifies whether the attribute is Required (R), Optional (O), or Conditional (C), in implementation based on the Device Function Code. Attributes that are not applicable for a device function code are denoted by a dash (-).
The Device Function Codes are:
- G – Regenerative (Active) AC/DC Converters (No Control Mode, No Control Method)
- N - Non-Regenerative (Passive) AC/DC Converters (No Control Mode, No Control Method
- E – Encoder, Feedback Only (No Control Mode, No Control Method)
- P – Position Loop (Position Control Mode, Closed Loop Vector Control Method)
- V – Velocity Loop (Velocity Control Mode, Closed Loop Vector Control Method)
- T – Torque Loop (Torque Control Mode, Closed Loop Vector Control Method)
- F – Frequency Control (Velocity Control Mode, Frequency Control Method)
- X – Track Section (No Control Mode, No Control Method)
The C/D column states whether the attribute is replicated in the drive.
Attr. ID | Access Rule | Tag | Attribute Name | G | N | E | F | P | V | T | C/D | Conditional Implementation | Axis Test Mode (Test Mode Configuration) |
---|---|---|---|---|---|---|---|---|---|---|---|---|---|
2011 | Get | T | AC Line Current | R | - | - | - | - | - | - | Yes | V32 | |
2034 | Set | AC Line Current Unbalance Limit | O | - | - | - | - | - | - | Yes | V32 | ||
2225 | Get | T | AC Line Electrical Angle | O | - | - | - | - | - | - | Yes | V32 | |
2010 | Get | T | AC Line Frequency | R | - | - | - | - | - | - | Yes | V32 | |
2245 | Set | AC Line Frequency Change Action | O | - | - | - | - | - | - | Yes | V32 | ||
2246 | Set | AC Line Frequency Change Threshold | O | - | - | - | - | - | - | Yes | V32 | ||
2247 | Set | AC Line Frequency Change Time | O | - | - | - | - | - | - | Yes | V32 | ||
2284 | Set | AC Line High Freq User Limit | O | - | - | - | - | - | - | Yes | V32 | ||
2286 | Set | AC Line High Freq User Limit - Alternate | O | - | - | - | - | - | - | Yes | V32 | ||
2285 | Set | AC Line Low Freq User Limit | O | - | - | - | - | - | - | Yes | V32 | ||
2287 | Set | AC Line Low Freq User Limit - Alternate | O | - | - | - | - | - | - | Yes | V32 | ||
2280 | Set | AC Line Overvoltage User Limit | O | - | - | - | - | - | - | Yes | V32 | ||
2282 | Set | AC Line Overvoltage User Limit - Alternate | O | - | - | - | - | - | - | Yes | V32 | ||
2041 | Set | AC Line Source Impedance | O | - | - | - | - | - | - | Yes | V32 | ||
2043 | Set | AC Line Source Impedance - Alternate | O | - | - | - | - | - | - | Yes | V32 | ||
2042 | Set | AC Line Source Power | O | - | - | - | - | - | - | Yes | V32 | ||
2044 | Set | AC Line Source Power - Alternate | O | - | - | - | - | - | - | Yes | V32 | ||
2040 | Set | AC Line Source Select | O | - | - | - | - | - | - | Yes | V32 | ||
1078 | Set | AC Line Sync Configuration | O | - | - | - | - | - | - | V36 | |||
2035 | Set | AC Line Sync Error Tolerance | O | - | - | - | - | - | - | Yes | V32 | ||
2037 | Set | AC Line Sync Ki | O | - | - | - | - | - | - | - | V36 | ||
2036 | Set | AC Line Sync Kp | O | - | - | - | - | - | - | - | V36 | ||
2248 | Set | AC Line Sync Loss Action | O | - | - | - | - | - | - | Yes | V32 | ||
2249 | Set | AC Line Sync Loss Time | O | - | - | - | - | - | - | Yes | V32 | ||
1079 | Set | AC Line Sync Resoning Damping Gain | O | - | - | - | - | - | - | V32 | |||
2281 | Set | AC Line Undervoltage User Limit | O | - | - | - | - | - | - | Yes | V32 | ||
2283 | Set | AC Line Undervoltage User Limit - Alternate | O | - | - | - | - | - | - | Yes | V32 | ||
2012 | Get | T | AC Line Voltage | R | - | - | - | - | - | - | Yes | V32 | |
2228 | Set | AC Line Voltage Low Pass Filter Bandwidth | O | - | - | - | - | - | - | V36 | |||
2242 | Set | AC Line Voltage Sag Action | O | - | - | - | - | - | - | Yes | V32 | ||
2241 | Set | AC Line Voltage Sag Threshold | O | - | - | - | - | - | - | Yes | V32 | ||
2241 | Set | AC Line Voltage Sag Time | O | - | - | - | - | - | - | Yes | V32 | ||
2014 | Set | AC Line Voltage Time Constant | O | - | - | - | - | - | - | Yes | V32 | ||
2033 | Set | AC Line Voltage Unbalance Limit | O | - | - | - | - | - | - | Yes | V32 | ||
483/138 | Get | T | Acceleration Feedback | - | - | R | - | R | R | R | Yes | ||
452 | Get | T | Acceleration Feedforward Command | - | - | - | - | R | R | - | Yes | ||
460/216 | Set | T | Acceleration Feedforward Gain | - | - | - | - | R | R | - | Yes | ||
367 | Get | T | Acceleration Fine Command | - | - | - | - | O | O | O | Yes | ||
485 | Set | Acceleration Limit | - | - | - | O | O | O | O | Yes | |||
482 | Get | T | Acceleration Reference | - | - | - | - | O | O | O | Yes | ||
481 | Set | T | Acceleration Trim | - | - | - | - | O | O | O | Yes | ||
1600 | Get | T | Accelerometer Feedback Device X | O | O | O | O | O | O | O | V35 | ||
1603 | Get | T | Accelerometer Feedback Device X-RMS | O | O | O | O | O | O | O | V35 | ||
1601 | Get | T | Accelerometer Feedback Device Y | O | O | O | O | O | O | O | V35 | ||
1604 | Get | T | Accelerometer Feedback Device Y-RMS | O | O | O | O | O | O | O | V35 | ||
1602 | Get | T | Accelerometer Feedback Device Z | O | O | O | O | O | O | O | V35 | ||
1605 | Get | T | Accelerometer Feedback Device Z-RMS | O | O | O | O | O | O | O | V35 | ||
2091 | Set | Active Current Command | O | - | - | - | - | - | - | Yes | V32 | ||
2106 | Get | T | Active Current Error | O | - | - | - | - | - | - | Yes | V32 | |
2118 | Get | T | Active Current Feedback | O | - | - | - | - | - | - | Yes | V32 | |
2094 | Set | Active Current Low Pass Filter Bandwidth | O | - | - | - | - | - | - | Yes | V32 | ||
2095 | Set | Active Current Notch Filter Frequency | O | - | - | - | - | - | - | Yes | V32 | ||
2096 | Set | Active Current Rate Limit | O | - | - | - | - | - | - | Yes | V32 | ||
2080 | Get | T | Active Current Reference | R | - | - | - | - | - | - | Yes | V32 | |
2082 | Get | T | Active Current Reference - Compensated | R | - | - | - | - | - | - | Yes | V32 | |
2081 | Get | T | Active Current Reference - Filtered | R | - | - | - | - | - | - | Yes | V32 | |
2104 | Get | T | Active Current Reference - Limited | R | - | - | - | - | - | - | Yes | V32 | |
2093 | Set | T | Active Current Trim | O | - | - | - | - | - | - | Yes | V32 | |
53 | Get | T | Actual Acceleration | - | - | R | R | R | R | R | |||
48 | Get | T | Actual Position | - | - | R | R | R | R | R | Controller Loop Back: V35 | ||
52 | Get | T | Actual Velocity | - | - | R | R | R | R | R | |||
1376 | Set | Actuator Diameter | - | - | C | C | C | C | C | Yes | (R) Controller only attribute, Motion Scaling Configuration set to Controller Scaling; (O) Drive replicated attribute, Motion Scaling Configuration set to Drive Scaling | ||
1377 | Set | Actuator Diameter Unit | - | - | C | C | C | C | C | Yes | (R) Controller only attribute, Motion Scaling Configuration set to Controller Scaling; (O) Drive replicated attribute, Motion Scaling Configuration set to Drive Scaling | ||
1374 | Set | Actuator Lead | - | - | C | C | C | C | C | Yes | (R) Controller only attribute, Motion Scaling Configuration set to Controller Scaling; (O) Drive replicated attribute, Motion Scaling Configuration set to Drive Scaling | ||
1375 | Set | Actuator Lead Unit | - | - | C | C | C | C | C | Yes | (R) Controller only attribute, Motion Scaling Configuration set to Controller Scaling; (O) Drive replicated attribute, Motion Scaling Configuration set to Drive Scaling | ||
1373 | Set | Actuator Type | - | - | C | C | C | C | C | Yes | (R) Controller only attribute, Motion Scaling Configuration set to Controller Scaling; (O) Drive replicated attribute, Motion Scaling Configuration set to Drive Scaling | ||
836 | Set | Adaptive Tuning Configuration | - | - | - | - | O | O | O | Yes | V26 | ||
844 | Get | T | Adaptive Tuning Gain Scaling Factor | - | - | - | - | O | O | O | Yes | V26 | |
732/267 | Get | T | Analog Input 1 | O | O | - | O | O | O | O | Yes | ||
733/268 | Get | T | Analog Input 2 | O | O | - | O | O | O | O | Yes | ||
734 | Set | T | Analog Output 1 | O | O | - | O | O | O | O | Yes | ||
735 | Set | T | Analog Output 2 | O | O | - | O | O | O | O | Yes | ||
150 | Set | Application Catalog Number | R | R | R | R | R | R | R | V34 | |||
148 | Set | Application Catalog Number Instance | R | R | R | R | R | R | R | V34 | |||
149F | Set | Application Catalog Number Version | R | R | R | R | R | R | R | V34 | |||
201 | Set | Application Type | - | - | - | - | R | R | - | ||||
164 | Get | T | Attribute Error Code | R | R | R | R | R | R | R | |||
165 | Get | T | Attribute Error ID | R | R | R | R | R | R | R | |||
873 | Set | Auto Sag Configuration | - | - | - | O | O | O | O | Yes | E, V26 | ||
874 | Set | Auto Sag Slip Increment | - | - | - | O | O | O | O | Yes | E, V26 | ||
875 | Set | Auto Sag Slip Time Limit | - | - | - | O | O | O | O | Yes | E, V26 | ||
876 | Set | Auto Sag Start | - | - | - | O | O | O | O | Yes | E, V26 | ||
51 | Get | T | Average Velocity | - | - | R | R | R | R | R | |||
81 | Set | Average Velocity Timebase | - | - | R | R | R | R | R | ||||
1 | Get | Axis Address | R | R | R | R | R | R | R | ||||
30 | Set | Axis Configuration | R | R | R | R | R | R | R | Optional Enumeration | Controller Loop Back: V35 | ||
12 | Get | Axis Configuration State | R | R | R | R | R | R | R | ||||
11 | Get | Axis Data Type | R | R | R | R | R | R | R | ||||
35 | Get | T | Axis Event Bits | R | R | R | R | R | R | R | |||
34 | Get | T | Axis Fault Bits | R | R | R | R | R | R | R | |||
19 | Set | Axis Features | R | R | R | R | R | R | R | Optional bit maps | Controller Loop Back: V35 | ||
106 | Set | Axis ID | R | R | R | R | R | R | R | ||||
2 | Get | Axis Instance | R | R | R | R | R | R | R | ||||
753 | Get | T | Axis Safety Alarms | - | - | O | O | O | O | O | Yes | V32 | |
754 | Get | T | Axis Safety Alarms - Mfg | - | - | O | O | O | O | O | Yes | V32 | |
988 | Get | T | Axis Safety Alarms - RA | - | - | O | O | O | O | O | Yes | V32 | |
986 | Get | T | Axis Safety Data A | - | - | - | O | O | O | O | Yes | V31 | Controller Loop Back: V36 |
987 | Get | T | Axis Safety Data B | - | - | - | O | O | O | O | Yes | V31 | Controller Loop Back: V36 |
763 | Get | T | Axis Safety Faults | - | - | O | O | O | O | O | Yes | V24 | Controller Loop Back: V36 |
985 | Get | T | Axis Safety Faults - RA | - | - | O | O | O | O | O | Yes | V31 | |
760 | Get | T | Axis Safety State | - | - | O | O | O | O | O | Yes | V24 | Controller Loop Back: V36 |
761 | Get | T | Axis Safety Status | - | - | O | O | O | O | O | Yes | V24 | Controller Loop Back: V36 |
984 | Get | T | Axis Safety Status - RA | - | - | O | O | O | O | O | Yes | V31 | |
13 | Get | Axis State | R | R | R | R | R | R | R | ||||
33 | Get | T | Axis Status Bits | R | R | R | R | R | R | R | |||
124 | Set | Axis Update Schedule | R | R | R | R | R | R | R | ||||
825 | Set | Backlash Compensation Window | - | - | - | - | O | - | - | Yes | |||
423 | Set | Backlash Reversal Offset | - | - | - | - | R | - | - | E | |||
593 | Set | Brake Prove Ramp Time | - | - | - | O | O | O | O | Yes | E, V26 | ||
594 | Set | Brake Slip Tolerance | - | - | - | O | O | O | O | Yes | E, V26 | ||
592 | Set | Brake Test Torque | - | - | - | O | O | O | O | Yes | E, V26 | ||
576 | Set | Break Frequency | - | - | - | R | - | - | - | Yes | Basic V/Hz only | ||
575 | Set | Break Voltage | - | - | - | R | - | - | - | Yes | Basic V/Hz only | ||
816 | Set | Bus Observer Bandwidth | O | - | - | - | - | - | - | Yes | Voltage Control only, V32 | ||
815 | Set | Bus Observer Configuration | O | - | - | - | - | - | - | Yes | Optional Enumeration Voltage Control only, V32 | ||
812 | Get | T | Bus Observer Current Estimate | O | - | - | - | - | - | - | Yes | Voltage Control only, V32 | |
817 | Set | Bus Observer Integrator Bandwidth | O | - | - | - | - | - | - | Yes | Voltage Control only, V32 | ||
811 | Get | T | Bus Observer Voltage Rate Estimate | O | - | - | - | - | - | - | Yes | Voltage Control only, V32 | |
255 | Set | Bus Overvoltage Operational Limit | - | - | - | - | R | R | R | V29 | |||
638/262 | Get | T | Bus Regulator Capacity | O | O | - | O | O | O | O | Yes | ||
2571 | Bus Voltage Droop Control Mode | O | - | - | - | - | - | - | Voltage Control Only, V36 | ||||
2572 | Bus Voltage Droop Full Load | O | - | - | - | - | - | - | Voltage Control Only, V36 | ||||
2573 | Bus Voltage Droop Gain No Load | O | - | - | - | - | - | - | Voltage Control Only, V36 | ||||
2575 | Bus Voltage Droop Minimum Bus Voltage | O | - | - | - | - | - | - | Voltage Control Only, V36 | ||||
2574 | Bus Voltage Droop Transition Current | O | - | - | - | - | - | - | Voltage Control Only, V36 | ||||
2054 | Get | T | Bus Voltage Error | R | - | - | - | - | - | - | Yes | Voltage Control only, V32 | |
2065 | Set | Bus Voltage Error Tolerance | O | O | - | - | - | - | - | Yes | Voltage Control only - G, V32 | ||
2066 | Set | Bus Voltage Error Tolerance Time | O | O | - | - | - | - | - | Yes | Voltage Control only - G, V32 | ||
2053 | Get | T | Bus Voltage Feedback | R | - | - | - | - | - | - | Yes | Voltage Control only, V32 | |
2063 | Set | Bus Voltage Integrator Bandwidth | R | - | - | - | - | - | - | Yes | Voltage Control only, V32 | ||
2062 | Set | Bus Voltage Loop Bandwidth | R | - | - | - | - | - | - | Yes | Voltage Control only, V32 | ||
2064 | Set | Bus Voltage Rate Limit | O | - | - | - | - | - | - | Yes | Voltage Control only, V32 | ||
2050 | Get | T | Bus Voltage Reference | R | O | - | - | - | - | - | Yes | Voltage Control only - G, V32 | |
2061 | Set | Bus Voltage Reference Source | O | - | - | - | - | - | - | Yes | V32 | ||
2060 | Set | T | Bus Voltage Set Point | R | O | - | - | - | - | - | Yes | Voltage Control only - G, V32 | |
8 | Set | C2C Connection Instance | R | R | R | R | R | R | R | ||||
7 | Set | C2C Map Instance | R | R | R | R | R | R | R | ||||
756 | Get | CIP APR Faults | - | - | C | - | C | C | C | Yes | (R) Controller only attribute, Motion Scaling Configuration set to Controller Scaling; (O) Drive replicated attribute, Motion Scaling Configuration set to Drive Scaling; V27; E | ||
905 | Get | T | CIP APR Faults - RA | - | - | C | - | C | C | C | Yes | (R) Controller only attribute, Motion Scaling Configuration set to Controller Scaling; (O) Drive replicated attribute, Motion Scaling Configuration set to Drive Scaling; V27; E | |
26 | Get | CIP Axis Alarm Log | R | R | R | R | R | R | R | ||||
127 | Get | CIP Axis Alarm Log Count | R | R | R | R | R | R | R | ||||
28 | Set | CIP Axis Alarm Log Reset | R | R | R | R | R | R | R | ||||
659 | Get | T | CIP Axis Alarms | O | O | O | O | O | O | O | Yes | Controller Loop Back: V36 | |
904 | Get | T | CIP Axis Alarms - RA | O | O | O | O | O | O | O | Yes | ||
746 | Get | T | CIP Axis Alarms 2 | O | O | O | O | O | O | O | Yes | V32 | |
927 | Get | T | CIP Axis Alarms 2 - RA | O | O | O | O | O | O | O | Yes | V32 | |
672 | Set | CIP Axis Exception Action | R | R | R | R | R | R | R | Yes | Optional Enumeration | ||
748 | Set | CIP Axis Exception Action 2 | R | O | O | O | O | O | O | Yes | Optional Enumeration V32 | ||
908 | Set | CIP Axis Exception Action - RA | R | R | R | R | R | R | R | Yes | Optional Enumeration | ||
909 | Set | CIP Axis Exception Action 2 - RA | R | O | O | O | O | O | O | Yes | Optional Enumeration V32 | ||
25 | Get | CIP Axis Fault Log | R | R | R | R | R | R | R | ||||
126 | Get | CIP Axis Fault Log Count | R | R | R | R | R | R | R | ||||
27 | Set | CIP Axis Fault Log Reset | R | R | R | R | R | R | R | ||||
657 | Get | T | CIP Axis Faults | R | R | R | R | R | R | R | Yes | ||
744 | Get | T | CIP Axis Faults 2 | R | O | O | O | O | O | O | Yes | V32 | |
903 | Get | T | CIP Axis Faults - RA | R | R | R | R | R | R | R | Yes | ||
926 | Get | T | CIP Axis Faults 2 - RA | R | O | O | O | O | O | O | Yes | V32 | |
653 | Get | T | CIP Axis I/O Status | R | R | R | R | R | R | R | Yes | ||
901 | Get | T | CIP Axis I/O Status - RA | R | R | R | R | R | R | R | Yes | ||
650 | Get | T | CIP Axis State | R | R | R | R | R | R | R | Yes | Controller Loop Back: V36 | |
651 | Get | T | CIP Axis Status | R | R | R | R | R | R | R | Yes | Controller Loop Back: V36 | |
740 | Get | T | CIP Axis Status 2 | R | O | O | O | O | O | O | Yes | V32 | Controller Loop Back: V36 |
900 | Get | T | CIP Axis Status - RA | R | R | R | R | R | R | R | Yes | ||
924 | Get | T | CIP Axis Status 2 - RA | R | O | O | O | O | O | O | Yes | V32 | |
152 | Set | CIP Controller Get Attribute Access Bits | R | R | R | R | R | R | R | V34 | |||
151 | Set | CIP Controller Set Attribute Access Bits | R | R | R | R | R | R | R | V34 | |||
168 | Set | CIP Controller Get Attr Update Bits | R | R | R | R | R | R | R | ||||
167 | Set | CIP Controller Set Attr Update Bits | R | R | R | R | R | R | R | ||||
154 | Set | CIP Drive Get Attribute Access Bits | R | R | R | R | R | R | R | V34 | |||
153 | Set | CIP Drive Set Attribute Access Bits | R | R | R | R | R | R | R | V34 | |||
674 | Get | T | CIP Initialization Faults | R | R | R | R | R | R | R | Yes | ||
910 | Get | T | CIP Initialization Faults- RA | R | R | R | R | R | R | R | Yes | ||
676 | Get | T | CIP Start Inhibits | R | R | R | R | R | R | R | Yes | ||
912 | Get | T | CIP Start Inhibits - RA | R | R | R | R | R | R | R | Yes | ||
617 | Set | Coasting Time Limit | - | - | - | O | O | O | O | Yes | V26 | ||
100 | Get | T | Command Acceleration | - | - | - | R | R | R | - | |||
96 | Get | T | Command Position | - | - | - | R | R | R | - | Controller Loop Back: V35 | ||
95 | Set* | T | Command Torque | - | - | - | - | - | R | R | |||
360 | Set | Command Update Delay Offset | - | - | - | - | R | R | - | E | |||
99 | Get | T | Command Velocity | - | - | - | R | R | R | - | |||
561 | Set | Commutation Offset | - | - | - | - | R | R | R | Yes | E; PM Motor only | ||
850 | Set | Commutation Offset Compensation | - | - | - | - | O | O | O | Yes | E; IPM Motor only, V29 | ||
563 | Set | Commutation Polarity | - | - | - | - | O | O | O | Yes | E; PM Motor only | ||
562 | Set | Commutation Self-Sensing Current | - | - | - | - | O | O | O | Yes | E; PM Motor only, AOP | ||
618 | Set | Connection Loss Stopping Action | - | - | - | O | O | O | O | Yes | O-Enum V31 1 = Current Decel Disable (X/O/V33)(F/O) 2 = Ramped Decel Disable (F/O)(P/O/V33)(V/O) 3 = Current Decel Hold (P/O)(V/O) 4 = Ramped Decel Hold (P/O/V33)(V/O) 128 = DC Injection Brake (F/O/V34)(P/O/V34)(V/O/V34)(T/O/V34) 129 = AC Injection Brake (F/O/V34)(P/O/V34)(V/O/V34)(T/O/V34) | ||
41 | Get | Control Method | R | R | R | R | R | R | R | Yes | Derived – Axis Config | ||
40 | Set* | Control Mode | R | R | R | R | R | R | R | Yes | Derived – Axis Config | ||
82 | Set | Conversion Constant | - | - | R | R | R | R | R | ||||
2030 | Set | Converter AC Input Frequency | O | - | - | - | - | - | - | Yes | V32 | ||
2031 | Set | Converter AC Input Phasing | O | - | - | - | - | - | - | Yes | V32 | ||
2032 | Set | Converter AC Input Voltage | O | - | - | - | - | - | - | Yes | V32 | ||
637 | Get | T | Converter Capacity | O | O | - | O | O | O | O | Yes | ||
1280 | Set | Converter Configuration | R | - | - | - | - | - | - | V32; Optional Enumeration | |||
2001 | Set* | Converter Control Mode | R | - | - | - | - | - | - | Yes | V32; Derived - Converter Config | ||
2231 | Set | Converter Current Integrator Bandwidth | O | - | - | - | - | - | - | Yes | V32 | ||
2103 | Get | T | Converter Current Limit Source | O | - | - | - | - | - | - | Yes | V32 | |
2230 | Set | Converter Current Loop Bandwidth | O | - | - | - | - | - | - | Yes | V32 | ||
1065 | Set | Converter Current Loop Bandwidth Base | R | - | - | - | - | - | - | V32 | |||
2322 | Set | Converter Current Loop Damping | O | - | - | - | - | - | - | Yes | V32 | ||
2321 | Set | Converter Current Loop Tuning Method | O | - | - | - | - | - | - | Yes | V32 | ||
2323 | Set | Converter Current Power Feedback | O | - | - | - | - | - | - | V36 | |||
2232 | Set | Converter Current Vector Limit | O | - | - | - | - | - | - | Yes | V32 | ||
1069 | Set | Converter DC Bus Capacitance | R | - | - | - | - | - | - | V32 | |||
2004 | Set | Converter Disable Delay | O | - | - | - | - | - | - | V36 | |||
709 | Set | Converter Ground Current User Limit | O | - | - | - | - | - | - | Yes | V32 | ||
2288 | Set | Converter Heatsink Overtemp User Limit | O | - | - | - | - | - | - | Yes | V32 | ||
2243 | Set | Converter Input Phase Loss Action | O | - | - | - | - | - | - | Yes | V32 | ||
2244 | Set | Converter Input Phase Loss Time | O | - | - | - | - | - | - | Yes | V32 | ||
887 | Converter Inverter Motor Power Limit Min | O | - | - | - | - | - | - | V36 | ||||
888 | Converter Inverter Regen Power Limit Max | O | - | - | - | - | - | - | V36 | ||||
2289 | Set | Converter Line Overload User Limit | O | - | - | - | - | - | - | Yes | V32 | ||
1049 | Set | Converter Model Time Constant | R | - | - | - | - | - | - | V32 | |||
1064 | Set | Converter Model Time Constant Base | R | - | - | - | - | - | - | V32 | |||
596 | Set | Converter Motoring Power Limit | O | O | - | - | - | - | - | Yes | V32 | ||
2100 | Get | T | Converter Operative Current Limit | O | - | - | - | - | - | - | Yes | V32 | |
605 | Get | T | Converter Output Current | O | O | - | O | O | O | O | Yes | V26 | |
606 | Get | T | Converter Output Power | O | O | - | O | O | O | O | Yes | V26 | |
2268 | Set | Converter Overload Action | O | - | - | - | - | - | - | Yes | Optional Enumeration V32 | ||
700 | Set | Converter Overtemperature User Limit | O | - | - | - | - | - | - | Yes | V32 | ||
921 | Set | Converter Pre-Charge Overload User Limit | O | - | - | - | - | - | - | Yes | V32 | ||
1066 | Set | Converter Rated Current | R | - | - | - | - | - | - | V32 | |||
1067 | Set | Converter Rated Peak Current | R | - | - | - | - | - | - | V32 | |||
1068 | Set | Converter Rated Voltage | R | - | - | - | - | - | - | V32 | |||
626 | Set | Converter Regenerative Power Limit | O | O | - | - | - | - | - | Yes | V32 | ||
2003 | Set | Converter Startup Method | O | - | - | - | - | - | - | Yes | V32 | Controller Loop Back: V35 | |
701 | Set | Converter Thermal Overload User Limit | O | - | - | - | - | - | - | Yes | V32 | ||
520 | Get | T | Current Command | - | - | - | - | R | R | R | Yes | ||
840 | Set | T | Current Disturbance | - | - | - | - | O | O | O | Yes | ||
527 | Get | T | Current Error | - | - | - | - | O | O | O | Yes | ||
529 | Get | T | Current Feedback | - | - | - | - | O | O | O | Yes | ||
522 | Get | T | Current Limit Source | - | - | - | O | O | O | O | Yes | F Support in V29 | |
524 | Get | T | Current Reference | - | - | - | - | O | O | O | Yes | ||
553 | Set | Current Vector Limit | - | - | - | O | O | O | O | Yes | |||
46 | Set | Cyclic Read Update List | R | R | R | R | R | R | R | Controller Loop Back: V36 | |||
47 | Set | Cyclic Write Update List | R | R | R | R | R | R | R | ||||
196 | Set | Damping Factor | R | - | - | - | R | R | R | ||||
2468 | Set | DBC High Voltage Threshold | O | - | - | - | - | - | - | Voltage Control only, V36 | |||
2467 | Set | DBC Low Voltage Threshold | O | - | - | - | - | - | - | Voltage Control only, V36 | |||
2466 | Set | DBC Mode | O | - | - | - | - | - | - | Voltage Control only, V36 | |||
2472 | Set | DBC Motoring Minimum Power Limit | O | - | - | - | - | - | - | Voltage Control only, V36 | |||
2470 | Set | DBC Motoring Nominal Power Limit | O | - | - | - | - | - | - | Voltage Control only, V36 | |||
2469 | Set | DBC Nominal Voltage Threshold | O | - | - | - | - | - | - | Voltage Control only, V36 | |||
2473 | Set | DBC Regenerative Minimum Power Limit | O | - | - | - | - | - | - | Voltage Control only, V36 | |||
2471 | Set | DBC Regenerative Nominal Power Limit | O | - | - | - | - | - | - | Voltage Control only, V36 | |||
607 | Get | DC Bus Input Current | - | - | - | O | O | O | O | V34 | |||
620/266 | Get | T | DC Bus Voltage | R | R | - | R | R | R | R | Yes | ||
870 | Set | DC Injection Brake Current | - | - | - | O | O | O | O | Yes | |||
872 | Set | DC Injection Brake Time | - | - | - | O | O | O | O | Yes | |||
486 | Set | Deceleration Limit | - | - | - | O | O | O | O | Yes | |||
730 | Get | T | Digital Inputs | O | O | - | O | O | O | O | Yes | ||
731 | Set | T | Digital Outputs | O | O | - | O | O | O | O | Yes | ||
105 | Set* | T | Direct Command Velocity | - | R | - | R | - | |||||
200 | Set | Drive Model Time Constant | - | - | - | - | R | R | R | ||||
253 | Set | Drive Model Time Constant Base | - | - | - | - | R | R | R | ||||
254 | Set | Drive Rated Peak Current | - | - | - | - | R | R | R | ||||
120 | Set | Dynamics Configuration Bits | - | - | - | R | R | R | - | ||||
1057 | Set | External DC Bus Capacitance | R | - | - | - | - | - | - | V32 | |||
1435 | Set | Feedback 1 Accel Filter Bandwidth | - | - | O | - | O | O | O | Yes | E | ||
2404 | Set | Feedback 1 Accel Filter Taps | - | - | O | - | O | O | O | Yes | E | ||
2405 | Set | Feedback 1 Battery Absolute | - | - | O | - | O | O | O | Yes | E; TG,NK | ||
2406 | Set | Feedback n Calibration Offset | O | O | O | E;TM, V33 | |||||||
1417 | Set | Feedback 1 Cycle Interpolation | - | - | R | - | R | R | R | Yes | E; Not Linear Displacement Transducer (feedback type), AOP | ||
1416 | Set | Feedback 1 Cycle Resolution | - | - | R | - | R | R | R | Yes | E; Not Linear Displacement Transducer (feedback type) | ||
1421 | Set | Feedback 1 Data Code | - | - | O | - | O | O | O | Yes | E; Digital Parallel (feedback type),SSI (feedback type) | ||
1420 | Set | Feedback 1 Data Length | - | - | O | - | O | O | O | Yes | E; Digital Parallel (feedback type),SSI (feedback type) | ||
1419 | Set | Feedback 1 Length | - | - | R | - | R | R | R | Yes | E; Linear Absolute Only | ||
2400 | Set | Feedback 1 Loss Action | - | - | O | - | O | O | O | Yes | E | ||
1414 | Set | Feedback 1 Polarity | - | - | O | - | O | O | O | Yes | E | ||
1425 | Set | Feedback 1 Resolver Cable Balance | - | - | O | - | O | O | O | Yes | E; Resolver (feedback type) | ||
1424 | Set | Feedback 1 Resolver Excitation Frequency | - | - | O | - | O | O | O | Yes | E; Resolver (feedback type) | ||
1423 | Set | Feedback 1 Resolver Excitation Voltage | - | - | O | - | O | O | O | Yes | E; Resolver (feedback type) | ||
1422 | Set | Feedback 1 Resolver Transformer Ratio | - | - | O | - | O | O | O | Yes | E; Resolver (feedback type) | ||
1401 | Get | Feedback 1 Serial Number | - | - | O | - | O | O | O | Yes | E | ||
1415 | Set | Feedback 1 Startup Method | - | - | R | - | R | R | R | Yes | E; Optional Enumeration | ||
1418 | Set | Feedback 1 Turns | - | - | R | - | R | R | R | Yes | E; Rotary Absolute Only | ||
1413 | Set | Feedback 1 Type | - | - | R | - | R | R | R | Yes | E; Optional Enumeration | ||
1411 | Set | Feedback 1 Unit | - | - | R | - | R | R | R | Yes | E | ||
1434 | Set | Feedback 1 Velocity Filter Bandwidth | - | - | O | - | O | O | O | Yes | E | ||
2403 | Set | Feedback 1 Velocity Filter Taps | - | - | O | - | O | O | O | Yes | E | ||
1485 | Set | Feedback 2 Accel Filter Bandwidth | - | - | O | - | O | O | O | Yes | E | ||
2454 | Set | Feedback 2 Accel Filter Taps | - | - | O | - | O | O | O | Yes | E | ||
2455 | Set | Feedback 2 Battery Absolute | - | - | O | - | O | O | O | Yes | E; TG, NK | ||
2456 | Set | Feedback 2 Calibration Offset | O | O | O | E; TM,V33 | |||||||
1467 | Set | Feedback 2 Cycle Interpolation | - | - | R | - | R | R | R | Yes | E; Not Linear Displacement Transducer (feedback type), AOP | ||
1466 | Set | Feedback 2 Cycle Resolution | - | - | R | - | R | R | R | Yes | E; Not Linear Displacement Transducer (feedback type) | ||
1471 | Set | Feedback 2 Data Code | - | - | O | - | O | O | O | Yes | E; Digital Parallel (feedback type),SSI (feedback type) | ||
1470 | Set | Feedback 2 Data Length | - | - | O | - | O | O | O | Yes | E; Digital Parallel (feedback type),SSI (feedback type) | ||
1469 | Set | Feedback 2 Length | - | - | R | - | R | R | R | Yes | E; Linear Absolute Only | ||
2450 | Set | Feedback 2 Loss Action | - | - | O | - | O | O | O | Yes | E | ||
1464 | Set | Feedback 2 Polarity | - | - | O | - | O | O | O | Yes | E | ||
1475 | Set | Feedback 2 Resolver Cable Balance | - | - | O | - | O | O | O | Yes | E; Resolver (feedback type) | ||
1474 | Set | Feedback 2 Resolver Excitation Frequency | - | - | O | - | O | O | O | Yes | E; Resolver (feedback type) | ||
1473 | Set | Feedback 2 Resolver Excitation Voltage | - | - | O | - | O | O | O | Yes | E; Resolver (feedback type) | ||
1472 | Set | Feedback 2 Resolver Transformer Ratio | - | - | O | - | O | O | O | Yes | E; Resolver (feedback type) | ||
1451 | Get | Feedback 2 Serial Number | - | - | - | - | O | O | O | Yes | E | ||
1465 | Set | Feedback 2 Startup Method | - | - | R | - | R | R | R | Yes | E; Optional Enumeration | ||
1468 | Set | Feedback 2 Turns | - | - | R | - | R | R | R | Yes | E; Rotary Absolute Only | ||
1463 | Set | Feedback 2 Type | - | - | R | - | R | R | R | Yes | E; Optional Enumeration | ||
1461 | Set | Feedback 2 Unit | - | - | R | - | R | R | R | Yes | E | ||
1484 | Set | Feedback 2 Velocity Filter Bandwidth | - | - | O | - | O | O | O | Yes | E | ||
2453 | Set | Feedback 2 Velocity Filter Taps | - | - | O | - | O | O | O | Yes | E | ||
250 | Set | Feedback Commutation Aligned | - | - | - | - | O | O | O | Yes | E; PM Motor only, Optional Enumeration | ||
31 | Set | Feedback Configuration | R | R | R | R | R | R | R | Optional Enumeration | |||
708 | Set | Feedback Data Loss User Limit | - | - | O | O | O | O | O | Yes | E | ||
42 | Set* | Feedback Mode | - | - | R | R | R | R | R | Yes | Derived - Fdbk Config | ||
706 | Set | Feedback Noise User Limit | - | - | O | O | O | O | O | Yes | E | ||
707 | Set | Feedback Signal Loss User Limit | - | - | O | O | O | O | O | Yes | E | ||
44 | Set | Feedback Unit Ratio | - | - | - | - | O | O | - | Yes | E | ||
871 | Set | Flux Braking Enable | - | - | - | O | O | O | O | Yes | Ind Motor only | ||
528 | Get | T | Flux Current Error | - | - | - | - | O | O | O | Yes | ||
530 | Get | T | Flux Current Feedback | - | - | - | - | O | O | O | Yes | ||
525 | Get | T | Flux Current Reference | - | - | - | - | O | O | O | Yes | ||
557 | Set | Flux Integral Time Constant | - | - | - | - | O | O | O | Yes | |||
556 | Set | Flux Loop Bandwidth | - | - | - | - | O | O | O | Yes | |||
558 | Set | Flux Up Control | - | - | - | O | O | O | O | Yes | Ind Motor only, Optional Enumeration | ||
559 | Set | Flux Up Time | - | - | - | O | O | O | O | Yes | Ind Motor only | ||
380 | Set | Flying Start Enable | - | - | - | O | - | O | - | Yes | |||
381 | Set | Flying Start Method | - | - | - | O | - | O | - | Yes | V29 | ||
570 | Set | Frequency Control Method | - | - | - | R | - | - | - | Yes | Optional Enumeration | ||
498 | Set | Friction Compensation Sliding | - | - | - | - | O | O | O | Yes | |||
499 | Set | Friction Compensation Static | - | - | - | - | O | O | O | Yes | |||
500 | Set | Friction Compensation Viscous | - | - | - | - | O | O | O | Yes | |||
826/421 | Set | Friction Compensation Window | - | - | - | - | O | - | - | Yes | |||
2528 | Set | Gain Optimization Time | - | - | - | - | O | O | - | ||||
189 | Set | Gain Tuning Configuration Bits | - | - | - | - | R | R | R | ||||
3 | Get | Group Instance | R | R | R | R | R | R | R | ||||
981/243 | Get | T | Guard Faults | - | - | O | O | O | O | Yes | |||
980/242 | Get | T | Guard Status | - | - | - | O | O | O | O | Yes | ||
88 | Set | Home Configuration Bits | - | - | R | - | R | R | R | E | |||
86 | Set | Home Direction | - | - | - | - | R | R | - | E | |||
18 | Get | Home Event Task | - | - | R | R | R | R | R | E | |||
85 | Set | Home Mode | - | - | R | - | R | R | R | E | |||
90 | Set | Home Offset | - | - | R | - | R | R | R | E | |||
89 | Set | Home Position | - | - | R | - | R | R | R | E | |||
113 | Set | Home Return Speed | - | - | - | - | R | R | - | E | |||
87 | Set | Home Sequence | - | - | R | - | R | R | R | Optional Enumeration; E | |||
112 | Set | Home Speed | - | - | - | - | R | R | - | E | |||
245 | Get | Hookup Test Commutation Offset | - | - | R | - | R | R | R | PM Motor only; E | |||
246 | Get | Hookup Test Commutation Polarity | - | - | R | - | R | R | R | PM Motor only; E | |||
109 | Set | Hookup Test Distance | - | - | R | - | R | R | R | E | |||
247 | Get | Hookup Test Feedback 1 Direction | - | - | R | - | R | R | R | E | |||
248 | Get | Hookup Test Feedback 2 Direction | - | - | R | - | R | R | R | E | |||
111 | Set | Hookup Test Feedback Channel | - | - | R | - | R | R | R | E | |||
244 | Get | Hookup Test Status | - | - | R | R | R | R | R | ||||
110 | Set | Hookup Test Time | - | - | - | R | - | R | - | !E | |||
1346 | Set | Induction Motor Flux Current | - | - | - | R | R | R | R | Yes | Ind Motor only | ||
1349 | Set | Induction Motor Magnetization Reactance | - | - | - | O | O | O | O | Yes | Ind Motor only | ||
1345 | Set | Induction Motor Rated Frequency | - | - | - | R | R | R | R | Yes | Ind Motor only | ||
1352 | Set | Induction Motor Rated Slip Speed | - | - | - | O | O | O | O | Yes | Ind Motor only | ||
1351 | Set | Induction Motor Rotor Leakage Reactance | - | - | - | O | O | O | O | Yes | Ind Motor only | ||
1350 | Set | Induction Motor Rotor Resistance | - | - | - | O | O | O | O | Yes | Ind Motor only | ||
1348 | Set | Induction Motor Stator Leakage Reactance | - | - | - | O | O | O | O | Yes | Ind Motor only | ||
1347 | Set | Induction Motor Stator Resistance | - | - | - | R | R | R | R | Yes | Ind Motor only | ||
20 | Set | Inhibit Axis | R | R | R | R | R | R | R | Controller Loop Back: V35 | |||
60 | Get | T | Interpolated Actual Position | - | - | R | - | R | R | R | E | ||
101 | Get | T | Interpolated Command Position | - | - | - | - | R | R | - | E | ||
108 | Set | Interpolated Position Configuration | - | - | R | - | R | R | R | E | |||
59 | Set | T | Interpolation Time | - | - | R | - | R | R | R | E | ||
636 | Get | T | Inverter Capacity | - | - | - | R | R | R | R | Yes | ||
2295 | Set | Inverter Ground Current User Limit | - | - | - | O | O | O | O | V34 | |||
647 | Set | Inverter Overload Action | - | - | - | O | O | O | O | Yes | Optional Enumeration | ||
699 | Set | Inverter Thermal Overload User Limit | - | - | - | O | O | O | O | Yes | |||
1338 | Set | Linear Motor Damping Coefficient | - | - | - | O | O | O | O | Yes | Linear Motor only | ||
2313 | Set | Linear Motor Integral Limit Switch | - | - | - | O | O | O | O | Yes | Linear Motor only | ||
1336 | Set | Linear Motor Mass | - | - | - | - | O | O | O | Yes | Linear Motor only | ||
1337 | Set | Linear Motor Max Speed | - | - | - | O | O | O | O | Yes | Linear Motor only | ||
1334 | Set | Linear Motor Pole Pitch | - | - | - | R | R | R | R | Yes | Linear Motor only | ||
1335 | Set | Linear Motor Rated Speed | - | - | - | R | R | R | R | Yes | Linear Motor only | ||
203 | Set | Load Coupling | - | - | - | - | R | R | R | ||||
352 | Set | Load Inertia Ratio | - | - | - | - | R | R | R | ||||
801 | Get | T | Load Observer Acceleration Estimate | - | - | - | - | O | O | O | Yes | ||
806 | Set | T | Load Observer Bandwidth | - | - | - | - | O | O | O | Yes | ||
805 | Set | Load Observer Configuration | - | - | - | - | O | O | O | Yes | Optional Enumeration | ||
809 | Set | Load Observer Feedback Gain | - | - | - | - | O | O | O | Yes | |||
807 | Set | T | Load Observer Integrator Bandwidth | - | - | - | - | O | O | O | Yes | ||
802 | Get | T | Load Observer Torque Estimate | - | - | - | - | O | O | O | Yes | ||
205 | Set | Load Ratio | - | - | - | - | R | R | R | ||||
1370 | Set | Load Type | - | - | C | C | C | C | C | Yes | (R) Controller only attribute Motion Scaling Configuration set to Controller Scaling; (O) Drive replicated attribute, Motion Scaling Configuration set to Drive Scaling | ||
750 | Set | Local Control | O | O | O | O | O | O | O | Yes | Optional Enumeration | ||
202 | Set | Loop Response | R | - | - | - | R | R | - | ||||
4 | Set | Map Instance | R | R | R | R | R | R | R | ||||
21 | Set | Master Input Configuration Bits | - | - | R | - | R | R | - | E | |||
102 | Get | T | Master Offset | - | - | - | R | R | R | - | |||
22 | Set | Master Position Filter Bandwidth | - | - | R | - | R | R | - | E | |||
115 | Set | Maximum Acceleration | - | - | - | R | R | R | - | ||||
118 | Set | Maximum Acceleration Jerk | - | - | - | R | R | R | - | ||||
116 | Set | Maximum Deceleration | - | - | - | R | R | R | - | ||||
119 | Set | Maximum Deceleration Jerk | - | - | - | R | R | R | - | ||||
573 | Set | Maximum Frequency | - | - | - | R | - | - | - | Yes | |||
114 | Set | Maximum Speed | - | - | - | R | R | R | - | ||||
572 | Set | Maximum Voltage | - | - | - | R | - | - | - | Yes | |||
614 | Set | Mechanical Brake Control | - | - | - | O | O | O | O | Yes | |||
616 | Set | Mechanical Brake Engage Delay | - | - | - | O | O | O | O | Yes | |||
615 | Set | Mechanical Brake Release Delay | - | - | - | O | O | O | O | Yes | |||
10 | Get | Memory Usage | R | R | R | R | R | R | R | ||||
9 | Get | Memory Use | R | R | R | R | R | R | R | ||||
159 | Get | T | Module Alarm Bits | R | R | R | R | R | R | R | |||
5 | Set | Module Channel | R | R | R | R | R | R | R | ||||
6 | Set | Module Class Code | R | R | R | R | R | R | R | ||||
163 | Get | T | Module Fault Bits | R | R | R | R | R | R | R | |||
23 | Get | T | Motion Alarm Bits | - | - | R | R | R | R | R | |||
29 | Set | Motion Exception Action | - | - | R | R | R | R | R | ||||
24 | Get | T | Motion Fault Bits | - | - | R | R | R | R | R | |||
79 | Set | Motion Polarity | - | - | R | R | R | R | R | Yes | Controller only attribute, Motion Scaling Configuration set to Controller Scaling; Drive replicated attribute, Motion Scaling Configuration set to Drive Scaling | ||
78 | Set | Motion Resolution | - | - | R | R | R | R | R | Yes | Controller only attribute, Motion Scaling Configuration set to Controller Scaling; Drive replicated attribute, Motion Scaling Configuration set to Drive Scaling | ||
45 | Set | Motion Scaling Configuration | - | - | R | R | R | R | R | Yes | Drive Scaling only; Optional Enumeration | ||
32 | Get | T | Motion Status Bits | - | - | R | R | R | R | R | |||
77 | Set | Motion Unit | - | - | R | R | R | R | R | Yes | Controller only attribute, Motion Scaling Configuration set to Controller Scaling; Drive replicated attribute, Motion Scaling Configuration set to Drive Scaling | ||
635/259 | Get | T | Motor Capacity | - | - | - | R | R | R | R | Yes | ||
251 | Set | Motor Catalog Number | R | - | - | - | R | R | R | Yes | (R) Controller only attribute !NV; (O) Drive replicated attribute, NV | ||
1313 | Set | Motor Data Source | - | - | - | R | R | R | R | Yes | Optional Enumeration | ||
1314 | Set | Motor Device Code | - | - | - | R | R | R | R | Yes | |||
523/263 | Get | T | Motor Electrical Angle | - | - | - | - | R | R | R | Yes | PM Motor only | |
1323 | Set | Motor Integral Thermal Switch | - | - | - | O | O | O | O | Yes | |||
1324 | Set | Motor Max Winding Temperature | - | - | - | O | O | O | O | Yes | |||
2460 | Set | Motor Stability Control Enable | - | - | - | - | O | - | O | O | V33 | ||
2461 | Set | Motor Stability Control Filter Bandwidth | - | - | - | - | O | - | O | O | V33 | ||
2463 | Set | Motor Stability Control Frequency Gain | - | - | - | - | O | - | O | O | V33 | ||
2462 | Set | Motor Stability Control Voltage Gain | - | - | - | - | O | - | O | O | V33 | ||
646 | Set | Motor Overload Action | - | - | - | O | O | O | O | Yes | Optional Enumeration | ||
1322 | Set | Motor Overload Limit | - | - | - | O | O | O | O | Yes | |||
695 | Set | Motor Overspeed User Limit | - | - | - | O | O | O | O | Yes | |||
694 | Set | Motor Phase Loss Limit | - | - | - | O | O | O | O | Yes | V26 | ||
1317 | Set | Motor Polarity | - | - | - | O | O | O | O | Yes | |||
1319 | Set | Motor Rated Continuous Current | - | - | - | R | R | R | R | Yes | |||
1321 | Set | Motor Rated Output Power | - | - | - | C | C | C | C | Yes | O-PM; R-IM | ||
1320 | Set | Motor Rated Peak Current | - | - | - | C | C | C | C | Yes | R-PM; O-IM | ||
1318 | Set | Motor Rated Voltage | - | - | - | R | R | R | R | Yes | |||
1000 | Get | Motor Test Bus Overvoltage Speed | - | - | - | R | R | R | R | IPM Motor Only, V29 | |||
1001 | Get | Motor Test Commutation Offset Comp | - | - | - | R | R | R | R | IPM Motor Only, V29 | |||
174 | Get | Motor Test Counter EMF | - | - | - | R | R | R | R | PM Motor only | |||
172 | Get | Motor Test Flux Current | - | - | - | R | R | R | R | Ind Motor only | |||
171 | Get | Motor Test Inductance | - | - | - | R | R | R | R | Ind, SPM Motor Only | |||
999 | Get | Motor Test Ld Flux Saturation | - | - | - | R | R | R | R | IPM Motor Only, V29 | |||
997 | Get | Motor Test Ld Inductance | - | - | - | R | R | R | R | IPM Motor Only, V29 | |||
998 | Get | Motor Test Lq Flux Saturation | - | - | - | R | R | R | R | IPM Motor Only, V29 | |||
996 | Get | Motor Test Lq Inductance | - | - | - | R | R | R | R | IPM Motor Only, V29 | |||
170 | Get | Motor Test Resistance | - | - | - | R | R | R | R | ||||
173 | Get | Motor Test Slip Speed | - | - | - | R | R | R | R | Ind Motor only | |||
175 | Get | Motor Test Status | - | - | - | R | R | R | R | ||||
697 | Set | Motor Thermal Overload User Limit | - | - | - | O | O | O | O | Yes | |||
1315 | Set | Motor Type | - | - | - | R | R | R | R | Yes | Optional Enumeration | ||
2540 | Set | Motor Voltage Feedback Offset Limit | O | O | O | V36, TAM Bit Valid and TAM is present | |||||||
2538 | Set | Motor Voltage Feedback Offset Mode | O | O | O | V36, TAM Bit Valid and TAM is present | |||||||
2537 | Set | Motor Voltage Feedback Source | O | O | O | V36, TAM Bit Valid and TAM is present | |||||||
2539 | Set | Motor Voltage Feedback Threshold | O | O | O | V36, TAM Bit Valid and TAM is present | |||||||
1316 | Set | Motor Unit | - | - | - | R | R | R | R | Yes | |||
1325 | Set | Motor Winding To Ambient Capacitance | - | - | - | O | O | O | O | Yes | |||
1326 | Set | Motor Winding To Ambient Resistance | - | - | - | O | O | O | O | Yes | |||
521 | Get | T | Operative Current Limit | - | - | - | O | O | O | O | Yes | F Support in V29 | |
14 | Get | Output Cam Execution Targets | - | - | R | R | R | R | R | E | |||
38 | Get | T | Output Cam Lock Status | - | - | R | - | R | R | R | E | ||
37 | Get | T | Output Cam Pending Status | - | - | R | - | R | R | R | E | ||
36 | Get | T | Output Cam Status | - | - | R | - | R | R | R | E | ||
39 | Get | T | Output Cam Transition Status | - | - | R | - | R | R | R | E | ||
601 | Get | T | Output Current | - | - | - | R | R | R | R | Yes | ||
600 | Get | T | Output Frequency | - | - | - | R | O | O | O | Yes | ||
603 | Get | T | Output Power | - | - | - | R | R | R | R | Yes | ||
602 | Get | T | Output Voltage | - | - | - | R | R | R | R | Yes | ||
508 | Set | Overtorque Limit | - | - | - | O | O | O | O | Yes | |||
509 | Set | Overtorque Limit Time | - | - | - | O | O | O | O | Yes | |||
1082 | Get | Planner Actual Position | - | - | R | R | R | R | R | V30 | |||
1081 | Get | Planner Command Position - Fractional | - | - | - | R | R | R | - | V30 | |||
1080 | Get | Planner Command Position - Integer | - | - | - | R | R | R | - | V30 | |||
1355 | Set | PM Motor Extended Speed Permissive | - | - | - | - | O | O | O | Yes | PM Motor only; V29 | ||
2310 | Set | PM Motor Flux Saturation | - | - | - | O | O | O | O | Yes | SPM Motor only | ||
1343 | Set | PM Motor Force Constant | - | - | - | O | O | O | O | Yes | Linear PM Motor only | ||
1328 | Set | PM Motor Inductance | - | - | - | R | R | R | R | Yes | SPM Motor only, LT Motors only | ||
2315 | Set | PM Motor Ld Flux Saturation | - | - | - | O | O | O | O | Yes | IPM Motor only, V29 | ||
1354 | Set | PM Motor Ld Inductance | - | - | - | O | O | O | O | Yes | IPM Motor only, V29 | ||
1358 | Set | PM Motor Linear Bus Overvoltage Speed | - | - | - | - | O | O | O | Yes | Linear PM Motor only; V29 | ||
1359 | Set | PM Motor Linear Max Extended Speed | - | - | - | - | O | O | O | Yes | Linear PM Motor only; V29 | ||
1344 | Set | PM Motor Linear Voltage Constant | - | - | - | R | R | R | R | Yes | Linear PM Motor only | ||
2314 | Set | PM Motor Lq Flux Saturation | - | - | - | O | O | O | O | Yes | IPM Motor only, V29 | ||
1353 | Set | PM Motor Lq Inductance | - | - | - | O | O | O | O | Yes | IPM Motor only, V29 | ||
1342 | Set | PM Motor Rated Force | - | - | - | O | O | O | O | Yes | Linear PM Motor only | ||
1339 | Set | PM Motor Rated Torque | - | - | - | O | O | O | O | Yes | Rotary PM Motor only | ||
1327 | Set | PM Motor Resistance | - | - | - | R | R | R | R | Yes | SPM,IPM, LTS Motor only | ||
1356 | Set | PM Motor Rotary Bus Overvoltage Speed | - | - | - | - | O | O | O | Yes | Rotary PM Motor only; V29 | ||
1357 | Set | PM Motor Rotary Max Extended Speed | - | - | - | - | O | O | O | Yes | Rotary PM Motor only; V29 | ||
1341 | Set | PM Motor Rotary Voltage Constant | - | - | - | R | R | R | R | Yes | Rotary PM Motor only | ||
1340 | Set | PM Motor Torque Constant | - | - | - | O | O | O | O | Yes | Rotary PM Motor only | ||
436/131 | Get | T | Position Error | - | - | - | - | R | - | - | Yes | ||
444/227 | Set | Position Error Tolerance | - | - | - | - | R | - | - | Yes | |||
445 | Set | Position Error Tolerance Time | - | - | - | - | O | - | - | Yes | |||
1402 | Get | T | Position Feedback 1 | - | - | R | - | R | R | R | Yes | E | |
1452 | Get | T | Position Feedback 2 | - | - | R | - | R | R | R | Yes | E | |
365 | Get | T | Position Fine Command | - | - | - | - | O | - | - | Yes | ||
442 | Set | T | Position Integrator Bandwidth | - | - | - | - | R | - | - | Yes | ||
446 | Set | Position Integrator Control | - | - | - | - | R | - | - | Yes | Optional bit maps | ||
437 | Get | T | Position Integrator Output | - | - | - | - | R | - | - | Yes | ||
447 | Set | Position Integrator Preload | - | - | - | - | O | - | - | Yes | |||
781 | Set | Position Lead Lag Filter Bandwidth | - | - | - | - | O | - | - | Yes | |||
782 | Set | Position Lead Lag Filter Gain | - | - | - | - | O | - | - | Yes | |||
443/228 | Set | Position Lock Tolerance | - | - | - | - | R | - | - | Yes | |||
441 | Set | T | Position Loop Bandwidth | - | - | - | - | R | - | - | Yes | ||
438 | Get | T | Position Loop Output | - | - | - | - | R | - | - | Yes | ||
783 | Set | Position Notch Filter Frequency | - | - | - | - | O | - | - | Yes | |||
432 | Get | T | Position Reference | - | - | - | - | R | - | - | Yes | ||
73 | Set | Position Scaling Denominator | - | - | R | R | R | R | R | ||||
72 | Set | Position Scaling Numerator | - | - | R | R | R | R | R | ||||
197 | Set | Position Servo Bandwidth | - | - | - | - | R | - | - | ||||
431 | Set | T | Position Trim | - | - | - | - | R | - | - | Yes | ||
80 | Set | Position Units | - | - | R | R | R | R | R | ||||
84 | Set | Position Unwind | - | - | R | - | R | R | R | Yes | Controller only attribute, Motion Scaling Configuration set to Controller Scaling; Drive replicated attribute, Motion Scaling Configuration set to Drive Scaling; E | ||
75 | Set | Position Unwind Denominator | - | - | R | - | R | R | R | E | |||
74 | Set | Position Unwind Numerator | - | - | R | - | R | R | R | E | |||
627 | Set | Power Loss Action | O | O | - | O | O | O | O | Yes | Optional Enumeration | ||
628 | Set | Power Loss Threshold | O | O | - | O | O | O | O | Yes | |||
630 | Set | Power Loss Time | O | O | - | O | O | O | O | Yes | |||
117 | Set | Programmed Stop Mode | R | R | R | R | R | R | R | ||||
590 | Set | Proving Configuration | - | - | - | O | O | O | O | Yes | V26 | ||
376 | Set* | Ramp Acceleration | - | - | - | O | - | O | - | Yes | |||
377 | Set* | Ramp Deceleration | - | - | - | O | - | O | - | Yes | |||
378 | Set | Ramp Jerk Control | - | - | - | O | - | O | - | Yes | |||
375 | Set* | Ramp Velocity - Negative | - | - | - | O | - | O | - | Yes | |||
374 | Set* | Ramp Velocity - Positive | - | - | - | O | - | O | - | Yes | |||
2092 | Set | Reactive Current Command | O | - | - | - | - | - | - | Yes | V32 | ||
2107 | Get | T | Reactive Current Error | O | - | - | - | - | - | - | Yes | V32 | |
2119 | Get | T | Reactive Current Feedback | O | - | - | - | - | - | - | Yes | V32 | |
2097 | Set | Reactive Current Rate Limit | O | - | - | - | - | - | - | Yes | V32 | ||
2083 | Get | T | Reactive Current Reference | R | - | - | - | - | - | - | Yes | V32 | |
2084 | Get | T | Reactive Current Reference - Compensated | R | - | - | - | - | - | - | Yes | V32 | |
2105 | Get | T | Reactive Current Reference - Limited | R | - | - | - | - | - | - | Yes | V32 | |
2002 | Set | Reactive Power Control | O | - | - | - | - | - | - | Yes | V32 | ||
2073 | Set | Reactive Power Rate Limit | O | - | - | - | - | - | - | Yes | V32 | ||
2070 | Set | Reactive Power Set Point | O | - | - | - | - | - | - | Yes | V32 | ||
16 | Get | Registration 1 Event Task | - | - | R | R | R | R | R | E | |||
63 | Get* | T | Registration 1 Negative Edge Position | - | - | R | - | R | R | R | Yes | E | |
67 | Get* | T | Registration 1 Negative Edge Time | - | - | R | - | R | R | R | Yes | E | |
55 | Get | T | Registration 1 Position | - | - | R | - | R | R | R | E | ||
62 | Get* | T | Registration 1 Positive Edge Position | - | - | R | - | R | R | R | Yes | E | |
66 | Get* | T | Registration 1 Positive Edge Time | - | - | R | - | R | R | R | Yes | E | |
57 | Get | T | Registration 1 Time | - | - | R | - | R | R | R | E | ||
17 | Get | Registration 2 Event Task | - | - | R | R | R | R | R | E | |||
65 | Get* | T | Registration 2 Negative Edge Position | - | - | R | - | R | R | R | Yes | E | |
69 | Get* | T | Registration 2 Negative Edge Time | - | - | R | - | R | R | R | Yes | E | |
56 | Get | T | Registration 2 Position | - | - | R | - | R | R | R | E | ||
64 | Get* | T | Registration 2 Positive Edge Position | - | - | R | - | R | R | R | Yes | E | |
68 | Get* | T | Registration 2 Positive Edge Time | - | - | R | - | R | R | R | Yes | E | |
58 | Get | T | Registration 2 Time | - | - | R | - | R | R | R | E | ||
356 | Set | Registration Inputs | - | - | R | - | R | R | R | AOP; E | |||
613/354 | Set | Resistive Brake Contact Delay | - | - | - | O | O | O | O | Yes | PM Motor only | ||
1333 | Set | Rotary Motor Damping Coefficient | - | - | - | O | O | O | O | Yes | Rotary Motor only | ||
2312 | Set | Rotary Motor Fan Cooling Derating | - | - | - | O | O | O | O | Yes | Rotary Motor only | ||
2311 | Set | Rotary Motor Fan Cooling Speed | - | - | - | O | O | O | O | Yes | Rotary Motor only | ||
1330 | Set | Rotary Motor Inertia | - | - | - | - | O | O | O | Yes | Rotary Motor only | ||
1332 | Set | Rotary Motor Max Speed | - | - | - | O | O | O | O | Yes | Rotary Motor only | ||
1329 | Set | Rotary Motor Poles | - | - | - | R | R | R | R | Yes | Rotary Motor only | ||
1331 | Set | Rotary Motor Rated Speed | - | - | - | R | R | R | R | Yes | Rotary Motor only | ||
578 | Set | Run Boost | - | - | - | R | - | - | - | Yes | Basic V/Hz and Fan/Pump V/Hz only | ||
766 | Set | Safe Stopping Action | - | - | - | O | O | O | O | Yes | V31 | ||
767 | Set | Safe Stopping Action Source | - | - | - | O | O | O | O | Yes | V31 | Controller Loop Back: V36 | |
765 | Set | Safe Torque Off Action | - | - | - | O | O | O | O | Yes | V26; Optional Enumeration | ||
759 | Set | Safe Torque Off Action Source | - | - | - | O | O | O | O | Yes | V31 | Controller Loop Back: V36 | |
758 | Set | Safety Fault Action | - | - | O | O | O | O | O | Yes | V32 | ||
70 | Set | Scaling Source | - | - | R | R | R | R | R | ||||
629 | Set | Shutdown Action | O | O | - | O | O | O | O | Yes | Optional Enumeration | ||
370 | Set | Skip Speed 1 | - | - | - | O | - | - | - | Yes | |||
371 | Set | Skip Speed 2 | - | - | - | O | - | - | - | Yes | |||
372 | Set | Skip Speed 3 | - | - | - | O | - | - | - | Yes | |||
373 | Set | Skip Speed Band | - | - | - | O | - | - | - | Yes | |||
833 | Set | SLAT Configuration | - | - | - | - | - | O | - | Yes | |||
834 | Set | SLAT Set Point | - | - | - | - | - | O | - | Yes | |||
835 | Set | SLAT Time Delay | - | - | - | - | - | O | - | Yes | |||
565 | Get | T | Slip Compensation | - | - | - | R | - | - | - | Yes | ||
566 | Set | Slip CompensationEnable | - | - | - | O | - | - | - | - | Ind Motor only, V36 | ||
94 | Set | Soft Travel Limit - Negative | - | - | R | - | R | R | R | E | |||
93 | Set | Soft Travel Limit - Positive | - | - | R | - | R | R | R | E | |||
92 | Set | Soft Travel Limit Checking | - | - | - | R | - | R | R | R | E | ||
50 | Get | T | Start Actual Position | - | - | R | R | R | R | R | |||
577 | Set | Start Boost | - | - | - | R | - | - | - | Yes | Basic V/Hz only | ||
98 | Get | T | Start Command Position | - | - | - | R | R | R | - | |||
104 | Get | T | Start Master Offset | - | - | - | R | R | R | - | |||
610 | Set | Stopping Action | - | - | - | R | R | R | R | Yes | Optional Enumeration | ||
612/338 | Set | Stopping Time Limit | - | - | - | O | O | O | O | Yes | |||
611/337 | Set | Stopping Torque | - | - | - | - | R | R | R | Yes | |||
49 | Get | T | Strobe Actual Position | - | - | R | R | R | R | R | |||
97 | Get | T | Strobe Command Position | - | - | - | R | R | R | - | |||
103 | Get | T | Strobe Master Offset | - | - | - | R | R | R | - | |||
252 | Set | System Acceleration Base | - | - | - | - | R | R | R | ||||
169 | Set | System Bandwidth | - | - | - | - | R | R | R | Derived – Servo BW | |||
2090 | Set | System Capacitance | R | - | - | - | - | - | - | Yes | Voltage Control only, V32 | ||
204 | Set | System Damping | - | - | - | - | R | R | R | Derived – Damp. Fact. | |||
496 | Set | T | System Inertia | - | - | - | - | R | R | O | Yes | ||
916 | Set | Test Mode Configuration | R | R | R | R | R | R | R | Device Test Mode V35 | Controller Loop Back: V35 | ||
917 | Set | Test Mode Enable | R | R | R | R | R | R | R | Device Test Mode V35 | Controller Loop Back: V35 | ||
555 | Set | Torque Integral Time Constant | - | - | - | - | O | O | O | Yes | |||
827 | Set | Torque Lead Lag Filter Bandwidth | - | - | - | - | O | O | O | Yes | |||
828 | Set | Torque Lead Lag Filter Gain | - | - | - | - | O | O | O | Yes | |||
505/333 | Set | T | Torque Limit - Negative | - | - | - | - | R | R | R | Yes | ||
504/332 | Set | T | Torque Limit - Positive | - | - | - | - | R | R | R | Yes | ||
554 | Set | Torque Loop Bandwidth | - | - | - | - | O | O | O | Yes | |||
502 | Set | T | Torque Low Pass Filter Bandwidth | - | - | - | - | O | O | O | Yes | ||
843 | Get | T | Torque Low Pass Filter Bandwidth Estimate | - | - | - | - | O | O | O | Yes | V26 | |
503 | Set | Torque Notch Filter Frequency | - | - | - | - | O | O | O | Yes | |||
841 | Get | T | Torque Notch Filter Frequency Estimate | - | - | - | - | O | O | O | Yes | V26 | |
837 | Set | Torque Notch Filter High Frequency Limit | - | - | - | - | O | O | O | Yes | V26 | ||
838 | Set | Torque Notch Filter Low Frequency Limit | - | - | - | - | O | O | O | Yes | V26 | ||
842 | Get | T | Torque Notch Filter Magnitude Estimate | - | - | - | - | O | O | O | Yes | V26 | |
839 | Set | Torque Notch Filter Tuning Threshold | - | - | - | - | O | O | O | Yes | V26 | ||
232 | Set | Torque Offset | - | - | - | - | R | R | R | ||||
591 | Set | Torque Prove Current | - | - | - | O | O | O | O | Yes | V26 | ||
506 | Set | Torque Rate Limit | - | - | - | - | O | O | O | Yes | |||
492 | Get | T | Torque Reference | - | - | - | - | R | R | R | Yes | ||
493 | Get | T | Torque Reference Filtered | - | - | - | - | R | R | R | Yes | ||
494 | Get | T | Torque Reference Limited | - | - | - | - | R | R | R | Yes | ||
507/334 | Set | Torque Threshold | - | - | - | - | O | O | O | Yes | |||
491 | Set | T | Torque Trim | - | - | - | - | R | R | R | Yes | ||
1056 | Set | Total DC Bus Capacitance | R | - | - | - | - | - | - | V32 | |||
206 | Set | Total Inertia | - | - | - | - | R | R | R | Rotary Motor only | |||
207 | Set | Total Mass | - | - | - | - | R | R | R | Linear Motor only | |||
1371 | Set | Transmission Ratio Input | - | - | C | C | C | C | C | Yes | (R) Controller only attribute, Motion Scaling Configuration set to Controller Scaling; (O) Drive replicated attribute, Motion Scaling Configuration set to Drive Scaling | ||
1372 | Set | Transmission Ratio Output | - | - | C | C | C | C | C | Yes | (R) Controller only attribute Motion Scaling Configuration set to Controller Scaling; (O) Drive replicated attribute, Motion Scaling Configuration set to Drive Scaling | ||
71 | Set | Travel Mode | - | - | R | R | R | R | R | Yes | Controller only attribute, Motion Scaling Configuration set to Controller Scaling; Drive replicated attribute, Motion Scaling Configuration set to Drive Scaling | ||
76 | Set | Travel Range | - | - | R | - | R | R | R | E | |||
181 | Get | Tune Acceleration | - | - | - | - | R | R | R | ||||
179 | Get | Tune Acceleration Time | - | - | - | - | R | R | R | ||||
182 | Get | Tune Deceleration | - | - | - | - | R | R | R | ||||
180 | Get | Tune Deceleration Time | - | - | - | - | R | R | R | ||||
187 | Set | Tune Friction | - | - | - | - | R | R | R | ||||
186 | Set | Tune Inertia Mass | - | - | - | - | R | R | R | ||||
188 | Set | Tune Load Offset | - | - | - | - | R | R | R | ||||
178 | Get | Tune Status | - | - | - | - | R | R | R | ||||
191 | Set | Tuning Direction | - | - | - | - | R | R | R | ||||
190 | Set | Tuning Select | - | - | - | - | R | R | R | ||||
194 | Set | Tuning Speed | - | - | - | - | R | R | R | ||||
195 | Set | Tuning Torque | - | - | - | - | R | R | R | ||||
193 | Set | Tuning Travel Limit | - | - | - | - | R | R | R | ||||
510 | Set | Undertorque Limit | - | - | - | O | O | O | O | Yes | |||
511 | Set | Undertorque Limit Time | - | - | - | O | O | O | O | Yes | |||
464/321 | Set | Velocity Droop | - | - | - | O | O | O | - | Yes | |||
455/135 | Get | T | Velocity Error | - | - | - | - | R | R | - | Yes | ||
465 | Set | Velocity Error Tolerance | - | - | - | - | O | O | - | Yes | |||
466 | Set | Velocity Error Tolerance Time | - | - | - | - | O | O | - | Yes | |||
454/134 | Get | T | Velocity Feedback | - | - | R | R | R | R | R | Yes | ||
1403 | Get | T | Velocity Feedback 1 | - | - | - | R | - | R | R | E, V34 | ||
1453 | Get | T | Velocity Feedback 2 | - | - | R | - | R | R | R | E, V34 | ||
433 | Get | T | Velocity Feedforward Command | - | - | - | - | R | - | - | Yes | ||
440/215 | Set | T | Velocity Feedforward Gain | - | - | - | - | R | - | - | Yes | ||
366 | Get | T | Velocity Fine Command | - | - | - | - | O | O | - | Yes | ||
462 | Set | T | Velocity Integrator Bandwidth | - | - | - | - | R | R | - | Yes | ||
467 | Set | Velocity Integrator Control | - | - | - | - | R | R | - | Yes | Optional bit maps | ||
456 | Get | T | Velocity Integrator Output | - | - | - | - | R | R | - | Yes | ||
468 | Set | Velocity Integrator Preload | - | - | - | - | O | O | - | Yes | |||
474/326 | Set | Velocity Limit - Negative | - | - | - | O | O | O | - | Yes | |||
473/325 | Set | Velocity Limit - Positive | - | - | - | O | O | O | - | Yes | |||
458 | Get | T | Velocity Limit Source | - | - | - | - | O | O | - | Yes | V29 | |
471 | Set | Velocity Lock Tolerance | - | - | - | O | O | O | - | Yes | |||
461 | Set | T | Velocity Loop Bandwidth | - | - | - | - | R | R | - | Yes | ||
457 | Get | T | Velocity Loop Output | - | - | - | - | R | R | - | Yes | ||
469 | Set | T | Velocity Low Pass Filter Bandwidth | - | - | - | - | O | O | - | Yes | ||
790 | Set | Velocity Negative Feedforward Gain | - | - | - | - | O | O | - | Yes | |||
231 | Set | Velocity Offset | - | - | - | - | R | R | - | ||||
453 | Get | T | Velocity Reference | - | - | - | R | R | R | - | Yes | ||
198 | Set | Velocity Servo Bandwidth | - | - | - | - | R | R | - | ||||
472/329 | Set | Velocity Standstill Window | - | - | R | R | R | R | R | Yes | |||
470/327 | Set | Velocity Threshold | - | - | O | O | O | O | O | Yes | |||
451 | Set | T | Velocity Trim | - | - | - | R | R | R | - | Yes | ||
589 | Set | Vertical Load Control | - | - | - | O | O | O | - | Yes | V31 | ||
15 | Get | Watch Event Task | - | - | R | R | R | R | R | E | |||
54 | Get | T | Watch Position | - | - | R | - | R | R | R | E | ||
608 | Set | Zero Speed | - | - | - | O | O | O | O | Yes | V26 | ||
609 | Set | Zero Speed Time | - | - | - | O | O | O | O | Yes | V26 |
Provide Feedback