Specify CIP Messages

Specify CIP Messages

The CIP Data Table Read and Write message types transfer data between
Logix 5000
controllers.
Select this command
If you want to
CIP Data Table Read
Read data from another controller.
The Source and Destination types must match.
CIP Data Table Write
Write data to another controller.
The Source and Destination types must match.
Reconfigure an I/O Module
Use the Module Reconfigure message to send new configuration information to an I/O module.
During the reconfiguration, the following occurs:
  • Input modules continue to send input data to the controller.
  • Output modules continue to control their output devices.
A Module Reconfigure message requires this configuration properties.
In this property
Select
Message Type
Module Reconfigure
Example
Follow these steps to reconfigure an I/O module.
  1. Set the required member of the configuration tag of the module to the new value.
  2. Send a Module Reconfigure message to the module.
    When reconfigure[5] is set, set the high alarm to 60 for the local module in slot 4. The Module Reconfigure message then sends the new alarm value to the module. The one shot instruction prevents the rung from sending multiple messages to the module while the reconfigure[5] is on.
    TIP:
    We recommend that you always include an XIO of the MSG.EN bit as an in-series MSG rung precondition.
Relay Ladder
RelayLadder_Pg284_v31
Structured Text
IF reconfigure[5] AND NOT reconfigure[6]THEN Local:4:C.Ch0Config.HAlarmLimit := 60;
IF NOT change_Halarm.EN THEN MSG(change_Halarm);
END_IF; END_IF;
reconfigure[6] := reconfigure[5];
Specify CIP Generic Messages
IMPORTANT:
ControlLogix modules have services that can be invoked by using a MSG instruction and choosing the CIP Generic message type.
If you want to
In this property
Type or select
Perform a pulse test on a digital output module
Message Type
CIP Generic
Service Type
Pulse Test
Source
tag_name of type INT [5]
This array contains
Description
tag_name[0]
Bit mask of points to test (test only one point at a time)
tag_name[1]
Reserved, leave 0
tag_name[2]
Pulse width (hundreds of Milli (mu), usually 20)
tag_name[3]
Zero cross delay for ControlLogix I/O (hundreds of Milli (mu), usually 40)
tag_name[4]
Verify delay
Destination
Blank
Get audit value
Message Type
CIP Generic
Service Type
Audit Value Get
Source Element
Cannot change this field, blank
Source Length
Cannot change this field, set to 0 bytes
Destination Element
This array contains
Description
tag_name of type DINT[2] or
LINT
This tag contains the Audit Value for the controller.
Important:
Rockwell Automation
recommends using the DINT[2] data type to avoid limitations when working with LINT data types in Allen-Bradley® controllers.
Get controller events monitored for changes
Message Type
CIP Generic
Service Type
Changes to Detect Get
Source Element
Cannot change this field, blank
Source Length
Cannot change this field, set to 0 bytes
Destination Element
This array contains
Description
tag_name of type DINT[2] or
LINT
This tag represents a bit mask of the changes monitored for the controller.
Important:
Rockwell Automation
recommends using the DINT[2] data type to avoid limitations when working with LINT data types in Allen-Bradley controllers.
Set controller events monitored for changes
Message Type
CIP Generic
Service Type
Changes to Detect Set
Source Element
This array contains
Description
tag_name of type DINT[2] or
LINT
This tag represents a bit mask of the changes monitored for the controller.
Important:
Rockwell Automation
recommends using the DINT[2] data type to avoid limitations when working with LINT data types in Allen-Bradley controllers.
Source Length
Cannot change this field, set to 8 bytes
Destination Element
Cannot change this field, blank
Reset electronic fuses on a digital output module
Message Type
CIP Generic
Service Type
Reset Electronic Fuse
Source
tag name of type DINT
This tag represents a bit mask of the points to reset fuses on.
Destination
Leave blank
Reset latched diagnostics on a digital input module
Message Type
CIP Generic
Service Type
Reset Latched Diagnostics (I)
Source
tag_name of type DINT
This tag represents a bit mask of the points to reset diagnostics on.
Reset latched diagnostics on a digital output module
Message Type
CIP Generic
Service Type
Reset Latched Diagnostics (O)
Source
tag_name of type DINT
This tag represents a bit mask of the points to reset diagnostics on.
Unlatch the alarm of an analog input module
Message Type
CIP Generic
Service Type
Select which alarm that you want to unlatch.
• Unlatch All Alarms (I)
• Unlatch Analog High Alarm (I)
• Unlatch Analog High High Alarm (I)
• Unlatch Analog Low Alarm (I)
• Unlatch Analog Low Low Alarm (I)
• Unlatch Rate Alarm (I)
Instance
Channel of the alarm to unlatch.
Unlatch the alarm of an analog output module
Message Type
CIP Generic
Service Type
Select which alarm that you want to unlatch.
• Unlatch All Alarms (O)
• Unlatch High Alarm (O)
• Unlatch Low Alarm (O)
• Unlatch Ramp Alarm (O)
Instance
Channel of the alarm to unlatch.
Get/Set Controller Events Monitored for Changes Bit Definitions
Tag Names
Data Type
Bit Definition
Get Controller Events Monitored for Changes
Set Controller Events Monitored for Changes
DINT[0]
Each bit has a specific meaning:
0 Store to removable media through Logix Designer application
1 Online edits were accepted, tested, or assembled
2 Partial import online transaction completed
3 SFC Forces were enabled
4 SFC Forces were disabled
5 SFC Forces were removed
6 SFC Forces were modified
7 I/O Forces were enabled
8 I/O Forces were disabled
9 I/O Forces were removed
10 I/O Forces were changed
11 Firmware update from unconnected source
12 Firmware update via removable media
13 Mode change via workstation
14 Mode change via mode switch
15 A major fault occurred
16 Major faults were cleared
7 Major faults were cleared via mode switch
118 Task properties were modified
19 Program properties were modified
20 Controller timeslice options were modified
21 Removable media was removed
22 Removable media was inserted
23 Safety signature created
24 Safety signature deleted
25 Safety lock
26 Safety unlock
27 Constant tag value changed
28 Constant tag multiple values changed
29 Constant tag attribute cleared
30 Tag set as constant
31 Custom log entry added
DINT[1]
32 Change that affects correlation
33 Helps protect signature in Run mode attribute set
34 Helps protect signature in Run mode attribute cleared
35…63 Unused
TIP:
  • Selecting the
    CIP Generic
    message type enables the
    Large Connection
    option on the
    Communication
    tab. Use large CIP Generic connections when a message is greater than 480 bytes. 500 bytes is typical, but there are headers at the front of the message. Large CIP connections are for messages up to 3980 bytes.
  • The
    Large Connection
    box is enabled only when the
    Connected
    box is checked and
    CIP Generic
    is selected as the message type on the
    Configuration
    tab.
  • The
    Large Connection
    option is available only in Logix Designer application, version 21.00.00 or later and RSLogix 5000 software, version 20.00.00 or later.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal