Autotune the PIDE Instruction

The
Logix Designer
application PIDE autotuner provides an open-loop autotuner built into the PIDE instruction. You can autotune from PanelView terminals or any other operator interface devices, as well as the
Logix Designer
application. The PIDE block has an Autotune Tag (type PIDE_AUTOTUNE) that you specify for those PIDE blocks that you want to autotune.
The PIDE autotuner is installed with the application, but you need an activation key to enable the autotuner. The autotuner is only supported in function block programming; it is not available in ladder diagram or structured text programming.
Use the
Autotune
tab to specify and configure the autotune tag for a PIDE block.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.