Structured Text Syntax

Structured Text Syntax

Structured text is a textual programming language that uses statements to define what to execute.
  • Structured text is not case sensitive.
  • Use tabs and carriage returns (separate lines) to make your structured text easier to read. They have no effect on the execution of the structured text.
Structured text is not case sensitive. Structured text can contain these components.
Term
Definition
Examples
Assignment
Use an assignment statement to assign values to tags. The := operator is the assignment operator.
Terminate the assignment with a semi colon ‘;.’
tag := expression;
Expression
An expression is part of a complete assignment or construct statement. An expression evaluates to a number (numerical expression), a String (string expression), or to a true or false state (BOOL expression)
Tag Expression
A named area of the memory where data is stored (BOOL, SINT, INT, DINT, REAL, String).
value1
Immediate Expression
A constant value
4
Operators Expression
A symbol or mnemonic that specifies an operation within an expression.
tag1 + tag2
tag1 >= value1
Function Expression
When executed, a function yields one value. Use parentheses to contain the operand of a function.
Even though their syntax is similar, functions differ from instructions in that functions can be used only in expressions. Instructions cannot be used in expressions.
function(tag1)
Instruction
An instruction is a standalone statement.
An instruction uses parentheses to contain its operands.
Depending on the instruction, there can be zero, one, or multiple operands.
When executed, an instruction yields one or more values that are part of a data structure. Terminate the instruction with a semi colon(;).
Even though their syntax is similar, instructions differ from functions in that instructions cannot be used in expressions. Functions can be used only in expressions.
instruction();
instruction(operand);
instruction(operand1, operand2,operand3);
Construct
A conditional statement used to trigger structured text code (that is, other statements). Terminate the construct with a semi colon (;).
IF...THEN CASE FOR...DO WHILE...DO
REPEAT...UNTIL
EXIT
Comment
Text that explains or clarifies what a section of structured text does.
Use comments to make it easier to interpret the structured text.
Comments do not affect the execution of the structured text.
Comments can appear anywhere in structured text.
//comment
(*start of comment . . . end of comment*)
/*start of comment . . . end of comment*/
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal