Attach Low Reference Signals - Input - FLEX I/O Calibration

Attach Low Reference Signals - Input - FLEX I/O Calibration

To attach low reference signals for offset calibration.
offset
The steady-state deviation of a controlled variable from a fixed set point. In a linear function (y=mx+b), the parameter (b) is used to drive the dependent variable (y) to zero when the independent variable (x) is zero.
  1. Attach a precision voltage/current source to the terminals.
  2. Set the precision voltage/current source to the correct value.
  3. Select
    Next
    to perform offset calibration.
The module reads the signal and calibrates.
You may also select:
  • Retry
    if an error occurs and you need to repeat a step in the calibration process.
    TIP:
    The button is only enabled with an error occurs.
  • Stop
    to cancel calibration and exit the calibration.
  • Help
    for assistance with this tab.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal