Input Offset for FLEX I/O Calibration

Input Offset for FLEX I/O Calibration

To view the results of the offset calibration:
offset
The steady-state deviation of a controlled variable from a fixed set point. In a linear function (y=mx+b), the parameter (b) is used to drive the dependent variable (y) to zero when the independent variable (x) is zero.
Look at the
Status
column. If
OK
appears, then select
Next
to perform the gain calibration.
You can also select:
  • Stop
    to cancel calibration and exit the calibration.
  • Help
    for assistance with this tab.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.