status

status

status
The condition of the circuit or system represented as logic 0 (Off) or logic 1 (On).
This term is also used to describe module status as follows:
This status:
Indicates:
Standby
a transient state that occurs when shutting down
Faulted
the controller is unable to communicate with the module
When the status is Faulted, the Connection tab displays the fault.
Validating
a transient state that occurs before connecting to the module
Connecting
a state that occurs while the connection(s) are being established to the module
Running
the module is communicating and everything is working as expected
Shutting Down
the connections are closing
Inhibited
the connection to the module is inhibited
Waiting
a connection to this module was not made for one of these reasons:
  • its parent did not make a connection to it
  • its parent is inhibited
  • its parent is faulted
Offline
not online
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal