Download dialog box

Use the
General
tab on the
Download
dialog box to confirm downloading the open project to the controller. Use the
Options
tab to prevent tag values in an online controller from being overwritten during a download.
ATTENTION:
Before a project is downloaded, the memory of the controller is cleared, so be certain that the correct controller is selected.
TIP: To open the Download dialog, select
Communications > Download
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.